WEP security key header.
#include <m2m_types.h>
Data Fields | |
uint8 | au8WepKey [WEP_104_KEY_SIZE] |
uint8 | u8KeyIndex |
uint8 | u8KeyLen |
uint8 | u8Rsv |
uint8 tstrM2mWifiWep::au8WepKey[WEP_104_KEY_SIZE] |
WEP Key represented in bytes (padded with 0's if WEP-40).
Referenced by m2m_wifi_connect_wep().
uint8 tstrM2mWifiWep::u8KeyIndex |
WEP Key Index.
Referenced by m2m_wifi_connect_wep().
uint8 tstrM2mWifiWep::u8KeyLen |
WEP Key Size.
Referenced by m2m_wifi_connect_wep().
uint8 tstrM2mWifiWep::u8Rsv |
Reserved for future use. Set to 0.