Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
WINC1500 Mode Change Example for SAMD21 XPlained Pro Documentation

Introduction

This example demonstrates the use of the WINC1500 with the SAMD21 Xplained Pro board to bring up as a station and then switch to an AP.
It uses the following hardware:

  • the SAMD21 Xplained Pro.
  • the WINC1500 on EXT1.

Main Files

  • main.c : Initialize the WINC1500. For the first time, the device act as station mode. Then switch to AP mode. For the details in each mode, refer to the MODE_STA and MODE_AP example.

Usage

  1. Configure below code in the main.h for AP information.
    * #define MAIN_WLAN_SSID "DEMO_AP"
    * #define MAIN_WLAN_AP_CHANNEL (6)
    *
  2. Build the program and download it into the board.
  3. On the computer, open and configure a terminal application as the follows.
    * Baud Rate : 115200
    * Data : 8bit
    * Parity bit : none
    * Stop bit : 1bit
    * Flow control : none
    *
  4. Start the application.
  5. In the terminal window, the following text should appear:
    * -- WINC1500 mode change example --
    * -- Compiled: xxx xx xxxx xx:xx:xx --
    * AP mode, start
    * AP mode, end
    *

Compilation Information

This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.

Contact Information

For further information, visit Microchip.