Here are listed all the functions that implement the Wlan Configuration APIs.
Functions | |
NMI_API sint8 | m2m_wifi_conf_auto_rate (tstrConfAutoRate *pstrConfAutoRate) |
Allow the host MCU app to configure auto TX rate selection algorithm. The application can use this API to tweak the algorithm performance. Moreover, it allows the application to force a specific WLAN PHY rate for transmitted data packets to favor range vs. throughput needs. More... | |
sint8 | m2m_wifi_get_mac_address (uint8 *pu8MacAddr) |
Request the current MAC address of the device (the working mac address). (the function is Blocking until response received) More... | |
sint8 | m2m_wifi_get_otp_mac_address (uint8 *pu8MacAddr, uint8 *pu8IsValid) |
Request the MAC address stored on the OTP (one time programmable) memory of the device. (the function is Blocking until response received) More... | |
sint8 | m2m_wifi_set_cust_InfoElement (uint8 *pau8M2mCustInfoElement) |
API to add or remove a user-defined Information Element. More... | |
sint8 | m2m_wifi_set_device_name (uint8 *pu8DeviceName, uint8 u8DeviceNameLength) |
Sets the WINC device name. The name string is used as a device name in DHCP hostname (option 12). More... | |
sint8 | m2m_wifi_set_gain_table_idx (uint8 u8GainTableIdx) |
set the gain table index corresponding to a specific WiFi region More... | |
sint8 | m2m_wifi_set_gains (tstrM2mWifiGainsParams *pstrM2mGain) |
Set the chip PPA gain for 11b/11gn. More... | |
sint8 | m2m_wifi_set_mac_address (uint8 au8MacAddress[6]) |
Synchronous API for assigning a MAC address to the WINC IC. More... | |
sint8 | m2m_wifi_set_tx_power (uint8 u8TxPwrLevel) |
set the TX power tenuM2mTxPwrLevel More... | |
NMI_API sint8 m2m_wifi_conf_auto_rate | ( | tstrConfAutoRate * | pstrConfAutoRate | ) |
Allow the host MCU app to configure auto TX rate selection algorithm. The application can use this API to tweak the algorithm performance. Moreover, it allows the application to force a specific WLAN PHY rate for transmitted data packets to favor range vs. throughput needs.
Configures WLAN automatic TX rate adaptation algorithm.
[in] | pstrConfAutoRate | The Auto rate configuration parameters as listed in tstrConfAutoRate. |
Allow the host MCU app to configure auto TX rate selection algorithm. The application can use this API to tweak the algorithm performance. Moreover, it allows the application to force a specific WLAN PHY rate for transmitted data packets to favor range vs. throughput needs.
[in] | pstrConfAutoRate | The Auto rate configuration parameters as listed in tstrConfAutoRate. |
References hif_send(), M2M_ERR_FAIL, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_CONG_AUTO_RATE, and NULL.
Request the current MAC address of the device (the working mac address). (the function is Blocking until response received)
Synchronous API to retrieve the MAC address currently in use by the device.
[out] | pu8MacAddr | Output MAC address buffer of 6 bytes size. |
Function to retrieve the current MAC address. The function is blocking until the response is received.
[out] | pu8MacAddr | Pointer to a buffer in memory containing a 6-byte MAC address (provided function returns M2M_SUCCESS). |
References hif_chip_sleep(), hif_chip_wake(), M2M_SUCCESS, and nmi_get_mac_address().
Request the MAC address stored on the OTP (one time programmable) memory of the device. (the function is Blocking until response received)
Synchronous API to query the MAC address programmed into the WINC ICs OTP memory.
[out] | pu8MacAddr | Output MAC address buffer of 6 bytes size. Valid only if *pu8Valid=1. |
[out] | pu8IsValid | A output boolean value to indicate the validity of pu8MacAddr in OTP. Output zero if the OTP memory is not programmed, non-zero otherwise. |
This function attempts to read the device's MAC address from the One Time Programmable (OTP) memory on the IC. The presence (yes or no) of a MAC address in the OTP memory and, in the case of it being present, its value is returned via RAM pointed to by the input arguments. Request the MAC address stored on the One Time Programmable(OTP) memory of the device. The function is blocking until the response is received.
[out] | pu8MacAddr | Output MAC address buffer 6 bytes in size. Valid only if *pu8Valid=1. |
[out] | pu8IsValid | A boolean value set by the callee to indicate the validity of pu8MacAddr in OTP. If no MAC has been programmed in the OTP the value of this parameter will be zero; otherwise it will be non-zero. |
References hif_chip_sleep(), hif_chip_wake(), M2M_SUCCESS, and nmi_get_otp_mac_address().
API to add or remove a user-defined Information Element.
Synchronous function to Add/Remove user-defined Information Element to the WIFIBeacon and Probe Response frames while chip mode is Access Point Mode.\n According to the information element layout shown bellow, if it is required to set new data for the information elements, pass in the buffer with the information according to the sizes and ordering defined bellow. However, if it's required to delete these IEs, fill the buffer with zeros.
[in] | pau8M2mCustInfoElement | Pointer to Buffer containing the IE to be sent. It is the application developer's responsibility to ensure on the correctness of the information element's ordering passed in. |
--------------- ---------- ---------- ------------------- -------- -------- ----------- ----------------------- | Byte[0] | Byte[1] | Byte[2] | Byte[3:length1+2] | ..... | Byte[n] | Byte[n+1] | Byte[n+2:lengthx+2] | |---------------|----------|----------|-------------------|-------- --------|-----------|---------------------| | #of all Bytes | IE1 ID | Length1 | Data1(Hex Coded) | ..... | IEx ID | Lengthx | Datax(Hex Coded) | --------------- ---------- ---------- ------------------- -------- -------- ----------- -----------------------
The example demonstrates how the information elements are set using this function.
References hif_send(), M2M_CUST_IE_LEN_MAX, M2M_ERR_FAIL, M2M_REQ_DATA_PKT, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_CUST_INFO_ELEMENT, and NULL.
Sets the WINC device name. The name string is used as a device name in DHCP hostname (option 12).
Asynchronous API to set the "Device Name" of the WINC IC.
[in] | pu8DeviceName | Buffer holding the device name. |
[in] | u8DeviceNameLength | Length of the device name. |
Sets the WINC device name. The name string is used as a device name in DHCP hostname (option 12). If a device is not set through this function a default name is assigned. The default name is WINC-XX-YY, where XX and YY are the last 2 octets of the OTP MAC address. If OTP (eFuse) is programmed, then the default name is WINC-00-00.
[in] | pu8DeviceName | Buffer holding the device name. Device name is a null terminated C string. |
[in] | u8DeviceNameLength | Length of the device name. Should not exceed the maximum device name's length M2M_DEVICE_NAME_MAX (including null character). |
References tstrM2MDeviceNameConfig::au8DeviceName, hif_send(), M2M_DEVICE_NAME_MAX, m2m_memcpy(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_SET_DEVICE_NAME, and NULL.
set the gain table index corresponding to a specific WiFi region
Set the Gain table index corresponding to specific WiFi region.
[in] | u8GainTableIdx | change the gain table index |
[in] | u8GainTableIdx | change the gain table index based on the WiFi region it is suppose to be used. |
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_SET_GAIN_TABLE_IDX, NULL, and tstrM2mWiFiGainIdx::u8GainTableIdx.
sint8 m2m_wifi_set_gains | ( | tstrM2mWifiGainsParams * | pstrM2mGain | ) |
Set the chip PPA gain for 11b/11gn.
[in] | pstrM2mGain | tstrM2mWifiGainsParams contain gain parameters as implemented in rf document. |
References hif_send(), M2M_ERR_FAIL, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_SET_GAINS, and NULL.
Synchronous API for assigning a MAC address to the WINC IC.
This function override the already assigned MAC address of the WINC board with a user provided one. This is for experimental use only and should never be used in the production SW.
[in] | au8MacAddress | MAC Address to be provisioned to the WINC. |
References tstrM2mSetMacAddress::au8Mac, hif_send(), m2m_memcpy(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_SET_MAC_ADDRESS, and NULL.
set the TX power tenuM2mTxPwrLevel
Set the TX power tenuM2mTxPwrLevel.
[in] | u8TxPwrLevel | change the TX power tenuM2mTxPwrLevel |
[in] | u8TxPwrLevel | Change the TX power based on the enumeration tenuM2mTxPwrLevel. |
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_SET_TX_POWER, NULL, and tstrM2mTxPwrLevel::u8TxPwrLevel.