AP Configuration.
This structure holds the configuration parameters for the M2M AP mode. It should be set by the application when it requests to enable the M2M AP operation mode. This mode supports either open, WEP or WPA/WPA2 mixed mode security types.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD16__ [2] |
uint8 | au8DHCPServerIP [4] |
uint8 | au8Key [M2M_MAX_PSK_LEN] |
uint8 | au8SSID [M2M_MAX_SSID_LEN] |
uint8 | au8WepKey [WEP_104_KEY_STRING_SIZE+1] |
uint8 | u8KeyIndx |
uint8 | u8KeySz |
uint8 | u8ListenChannel |
uint8 | u8SecType |
uint8 | u8SsidHide |
uint8 tstrM2MAPConfig::__PAD16__[2] |
Padding bytes for forcing alignment
uint8 tstrM2MAPConfig::au8DHCPServerIP[4] |
Ap IP server address
Referenced by m2m_wifi_start_provision_mode().
uint8 tstrM2MAPConfig::au8Key[M2M_MAX_PSK_LEN] |
WPA key
uint8 tstrM2MAPConfig::au8SSID[M2M_MAX_SSID_LEN] |
< Configuration parameters for the WiFi AP.AP SSID
Referenced by run_provisioning().
uint8 tstrM2MAPConfig::au8WepKey[WEP_104_KEY_STRING_SIZE+1] |
Wep key
uint8 tstrM2MAPConfig::u8KeyIndx |
Wep key Index
uint8 tstrM2MAPConfig::u8KeySz |
Wep/WPA key Size
uint8 tstrM2MAPConfig::u8ListenChannel |
Wi-Fi RF Channel which the AP will operate on
uint8 tstrM2MAPConfig::u8SecType |
Security type: Open, WEP or WPA/WPA2 mixed mode
uint8 tstrM2MAPConfig::u8SsidHide |
SSID Status "Hidden(1)/Visible(0)"