Specifies the macros and defines used by the Wlan APIs.
Modules | |
DebugDefines | |
#define DEFAULT_CONF_AR_INITIALIZER { 5, 1, TX_RATE_AUTO, TX_RATE_AUTO, 10, 5, 3 } |
#define M2M_802_1X_MSCHAP2_FLAG 0x01 |
Flag to indicate 802.1x MsChapV2 credentials: domain/user-name/password.
Referenced by m2m_wifi_connect_1x_mschap2().
#define M2M_802_1X_PREPEND_DOMAIN_FLAG 0x40 |
Flag to indicate that the 802.1x domain name should be prepended to the user-name: "Domain\Username". If the flag is not set then domain name is appended to the user-name: "Username@Domain". (Note that the '@' or '\' must be included in the domain name.)
Referenced by m2m_wifi_connect_1x_mschap2(), and m2m_wifi_connect_1x_tls().
#define M2M_802_1X_TLS_CLIENT_CERTIFICATE 1 |
Info type used in tstrM2mWifiAuthInfoHdr to indicate Enterprise TLS client certificate.
Referenced by m2m_wifi_connect_1x_tls().
#define M2M_802_1X_TLS_FLAG 0x02 |
Flag to indicate 802.1x TLS credentials: domain/user-name/private-key/certificate.
Referenced by m2m_wifi_connect_1x_tls().
#define M2M_802_1X_UNENCRYPTED_USERNAME_FLAG 0x80 |
Flag to indicate that the 802.1x user-name should be sent (unencrypted) in the initial EAP identity response. Intended for use with EAP-TLS only.
Referenced by m2m_wifi_connect_1x_mschap2(), and m2m_wifi_connect_1x_tls().
#define M2M_AP_CMD_BASE 70 |
The base value of all the Access Point mode host commands opcodes.
#define M2M_AUTH_1X_CERT_LEN_MAX 1584 |
The maximum length (in bytes) of certificate for authentication with Enterprise TLS methods.
Referenced by m2m_wifi_connect_1x_tls().
#define M2M_AUTH_1X_PASSWORD_LEN_MAX 256 |
The maximum length (in ASCII characters) of password for authentication with Enterprise MSCHAPv2 methods.
Referenced by m2m_wifi_connect_1x_mschap2().
#define M2M_AUTH_1X_PRIVATEKEY_LEN_MAX 256 |
The maximum length (in bytes) of private key modulus for authentication with Enterprise TLS methods. Private key exponent must be the same length as modulus, pre-padded with 0s if necessary.
Referenced by m2m_wifi_connect_1x_tls().
#define M2M_AUTH_1X_USER_LEN_MAX 100 |
The maximum length (in ASCII characters) of domain name + username (including '@' or '\') for authentication with Enterprise methods.
Referenced by m2m_wifi_connect_1x_mschap2(), and m2m_wifi_connect_1x_tls().
#define M2M_BUFFER_MAX_SIZE (1600UL - 4) |
Maximum size for the shared packet buffer.
#define M2M_CONFIG_CMD_BASE 1 |
The base value of all the host configuration commands opcodes.
#define M2M_CRED_ENCRYPT_FLAG 0x02 |
Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials should be encrypted when stored in WINC flash.
Referenced by m2m_wifi_connect_prepare_msg().
#define M2M_CRED_IS_ENCRYPTED_FLAG 0x20 |
Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials are encrypted in WINC flash. May only be set by WINC firmware.
#define M2M_CRED_IS_STORED_FLAG 0x10 |
Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials are stored in WINC flash. May only be set by WINC firmware.
#define M2M_CRED_STORE_FLAG 0x01 |
Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials should be stored in WINC flash.
Referenced by m2m_wifi_connect_prepare_msg().
#define M2M_CRYPTO_CMD_BASE 1 |
The base value of all the crypto mode host commands opcodes. The crypto Have special group so can extended from 1-M2M_MAX_GRP_NUM_REQ
#define M2M_CUST_IE_LEN_MAX 252 |
The maximum size of IE (Information Element).
Referenced by m2m_wifi_set_cust_InfoElement().
#define M2M_DEVICE_NAME_MAX 48 |
Maximum Size for the device name including the NULL termination.
Referenced by m2m_wifi_set_device_name().
#define M2M_ETHERNET_HDR_LEN 14 |
Length of the Ethernet header in bytes.
Referenced by m2m_wifi_send_ethernet_pkt().
#define M2M_ETHERNET_HDR_OFFSET 34 |
The offset of the Ethernet header within the WLAN Tx Buffer.
Referenced by m2m_wifi_send_ethernet_pkt().
#define M2M_FASTCONNECT_DEFAULT_RSSI_THRESH (-45) |
The default threshold RSSI for fast reconnection to an AP.
#define M2M_GEN_CMD_BASE 105 |
The base value of additional host wifi command opcodes. Usage restrictions (eg STA mode only) should always be made clear at the API layer in any case.
#define M2M_LISTEN_INTERVAL 1 |
The STA uses the Listen Interval parameter to indicate to the AP how many beacon intervals it shall sleep before it retrieves the queued frames from the AP.
Referenced by main().
#define M2M_MAC_ADDRES_LEN 6 |
The size of the 802 MAC address.
Referenced by m2m_wifi_connect_prepare_msg().
#define M2M_MAX_GRP_NUM_REQ (127) |
max number of request in one group equal to 127 as the last bit reserved for config or data pkt
#define M2M_MAX_PSK_LEN 65 |
1 more than the WPA PSK length (in ASCII format). This matches the size of the WPA PSK/Passphrase buffer (max ASCII contents + 1-byte length field). Alternatively it matches the WPA PSK length (in ASCII format) + 1 byte NULL termination.
Referenced by m2m_validate_ap_parameters(), m2m_wifi_connect_psk(), and m2m_wifi_connect_sc().
#define M2M_MAX_SSID_LEN 33 |
1 more than the max SSID length. This matches the size of SSID buffers (max SSID length + 1-byte length field).
Referenced by m2m_validate_ap_parameters(), m2m_wifi_connect_prepare_msg(), m2m_wifi_connect_sc(), m2m_wifi_delete_sc(), and m2m_wifi_request_scan_ssid_list().
#define M2M_MIN_PSK_LEN 9 |
1 more than the minimum WPA PSK Passphrase length. It matches the minimum WPA PSK Passphrase length + 1 byte NULL termination.
Referenced by m2m_validate_ap_parameters().
#define M2M_NTP_MAX_SERVER_NAME_LENGTH 32 |
Maximum NTP server name length
Referenced by m2m_wifi_configure_sntp().
#define M2M_OTA_CMD_BASE 100 |
The base value of all the OTA mode host commands opcodes. The OTA Have special group so can extended from 1-M2M_MAX_GRP_NUM_REQ
#define M2M_SCAN_DEFAULT_NUM_PROBE (2) |
The default number of probes per scan slot.
Referenced by m2m_validate_scan_options().
#define M2M_SCAN_DEFAULT_NUM_SLOTS (2) |
The default number of scan slots used by the WINC board.
#define M2M_SCAN_DEFAULT_PASSIVE_SLOT_TIME (300) |
The passive scan slot default duration in ms.
#define M2M_SCAN_DEFAULT_SLOT_TIME (30) |
The default duration in miliseconds of an active scan slot used by the WINC board.
#define M2M_SERVER_CMD_BASE 100 |
The base value of all the power save mode host commands codes.
#define M2M_SHA256_CONTEXT_BUFF_LEN (128) |
sha256 context size
#define M2M_STA_CMD_BASE 40 |
The base value of all the station mode host commands opcodes.
#define M2M_WIFI_CONN_BSSID_FLAG 0x01 |
Flag used in tstrM2mConnCredCmn to indicate that Wi-Fi connection must be restricted to an AP with a certain BSSID.
Referenced by m2m_wifi_connect_prepare_msg().
#define MAX_HIDDEN_SITES 4 |
max number of hidden SSID supported by scan request
Referenced by m2m_wifi_request_scan_ssid_list().
#define PSK_CALC_LEN 40 |
PSK is 32 bytes generated either:
#define PWR_DEFAULT PWR_HIGH |
#define TLS_CERTS_CHUNKED_SIG_VALUE 0x6ec8 |
Referenced by m2m_ssl_send_certs_to_winc().
#define TLS_CRL_DATA_MAX_LEN 64 |
#define TLS_CRL_MAX_ENTRIES 10 |
#define TLS_CRL_TYPE_CERT_HASH 1 |
#define TLS_CRL_TYPE_NONE 0 |
#define TLS_FILE_NAME_MAX 48 |
Maximum length for each TLS certificate file name including null terminator.
#define TLS_SRV_SEC_MAX_FILES 8 |
Maximum number of certificates allowed in TLS_SRV section.
#define TLS_SRV_SEC_START_PATTERN_LEN 8 |
Length of certificate struct start pattern.
#define WEP_104_KEY_SIZE ((uint8)13) |
The size in bytes of a 104-bit wep key.
#define WEP_104_KEY_STRING_SIZE ((uint8)26) |
The string length of a 104-bit wep key.
Referenced by m2m_validate_ap_parameters(), and m2m_wifi_connect_wep().
#define WEP_40_KEY_SIZE ((uint8)5) |
The size in bytes of a 40-bit wep key.
#define WEP_40_KEY_STRING_SIZE ((uint8)10) |
The string length of a 40-bit wep key.
Referenced by m2m_validate_ap_parameters(), and m2m_wifi_connect_wep().
#define WEP_KEY_MAX_INDEX ((uint8)4) |
WEP key index is in the range 1 to 4 inclusive. (This is decremented to result in an index in the range 0 to 3 on air.)
Referenced by m2m_validate_ap_parameters(), and m2m_wifi_connect_wep().
#define WLAN_11B_RATES_INITIALIZER |
#define WLAN_11BG_RATES_ASC_INITIALIZER |
#define WLAN_11BGN_RATES_ASC_INITIALIZER |
#define WLAN_11G_RATES_INITIALIZER |
#define WLAN_11N_RATES_INITIALIZER |