Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs.
Functions | |
sint8 | m2m_wifi_disable_ap (void) |
Synchronous API to disable access point mode on the WINC IC. More... | |
sint8 | m2m_wifi_enable_ap (CONST tstrM2MAPConfig *pstrM2MAPConfig) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC. More... | |
sint8 | m2m_wifi_enable_ap_ext (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC with extended options. More... | |
Synchronous API to disable access point mode on the WINC IC.
Must be called only when the AP is enabled through the @ref m2m_wifi_enable_ap function. Otherwise the call to this function will not be useful.
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_DISABLE_AP, and NULL.
Referenced by socket_cb().
NMI_API sint8 m2m_wifi_enable_ap | ( | CONST tstrM2MAPConfig * | pstrM2MAPConfig | ) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC.
The WINC IC supports the ability to operate as an access point with the following limitations: - Only 1 station may be associated at any given time. - Open system and WEP are the only security suites supported.
[in] | pstrM2MAPConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.
References tstrM2MAPConfigExt::au8DefRouterIP, tstrM2MAPConfigExt::au8DNSServerIP, tstrM2MAPConfigExt::au8SubnetMask, m2m_memcpy(), m2m_wifi_enable_ap_ext(), tstrM2MAPModeConfig::strApConfig, and tstrM2MAPModeConfig::strApConfigExt.
Referenced by main().
NMI_API sint8 m2m_wifi_enable_ap_ext | ( | CONST tstrM2MAPModeConfig * | pstrM2MAPModeConfig | ) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC with extended options.
The WINC IC supports the ability to operate as an access point with the following limitations: - Only 1 station may be associated at any given time. - Open system and WEP are the only security suites supported.
[in] | pstrM2MAPModeConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.
References hif_send(), M2M_ERR_FAIL, M2M_REQ_DATA_PKT, M2M_REQ_GROUP_WIFI, M2M_SUCCESS, m2m_validate_ap_parameters(), M2M_WIFI_REQ_ENABLE_AP, and NULL.
Referenced by m2m_wifi_enable_ap().