Introduction
This example demonstrates the use of the WINC1500 with the SAM Xplained Pro board to connect to a secured WEP, WPA network.
It uses the following hardware:
- the SAM Xplained Pro.
- the WINC1500 on EXT1.
Main Files
- main.c : Initialize the WINC1500 and connect AP using Security mode WEP, WPA.
Usage
- Assemble the devices and connect to USB debug cable from PC.
- On the computer, open and configure a terminal application as the follows.
* Baud Rate : 115200
* Data : 8bit
* Parity bit : none
* Stop bit : 1bit
* Flow control : none
*
- Prepare an AP that supports WEP and WPA/WPA2 Security and configure Wi-Fi Security. For more information, please refer to manufacturer's manual.
- To test WPA Security, Use case 2 in main function and modify MAIN_WLAN_PSK in source file "main.h".
- To test WEP Security, Use case 1 in main function and select wep64_parameters or wep128_parameters as security parameters. Modify MAIN_WLAN_DEVICE_NAME, MAIN_WLAN_WEP_KEY_INDEX and MAIN_WLAN_WEP_KEY_40 or MAIN_WLAN_WEP_KEY_104 in source file "main.h".
- Run the application. If the device connected successfully, IP address which is assigned by DHCP will be displayed on the terminal program
* -- WINC1500 security connection with WEP,WPA security example --
* -- Compiled: xxx xx xxxx xx:xx:xx --
* Connecting to XXXXXX.
* Wi-Fi connected
* Wi-Fi IP is xxx.xxx.xxx.xxx
*
Compilation Information
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.
Contact Information
For further information, visit Microchip.