Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
WINC1500 Connecting a Secured AP Using WPS Example for SAMD21 XPlained Pro Documentation

Introduction

This example demonstrates the use of the WINC1500 with the SAMD21 Xplained Pro board to connect to AP with WPS Security.
It uses the following hardware:

  • the SAMD21 Xplained Pro.
  • the WINC1500 on EXT1.

Main Files

  • main.c : Initialize the WINC1500 and connect AP using WPS.

Usage

  1. Assemble the devices and connect to USB debug cable from PC.
  2. On the computer, open and configure a terminal application as the follows.
    * Baud Rate : 115200
    * Data : 8bit
    * Parity bit : none
    * Stop bit : 1bit
    * Flow control : none
    *
  3. Prepare an AP that supports Wi-Fi Protected Setup(WPS)
  4. To test WPS button method, Use case 1 in main function.
  5. Configure below code in the main.h for WPS push button feature.
    *
  6. Press WPS button at the AP. ( For more information, please refer to AP product documentation )
  7. Run the application. The WINC1500 will be connected to the AP automatically without security information.
    * -- WINC1500 security connection with Wi-Fi Protected Setup(WPS) example --
    * -- Compiled: xxx xx xxxx xx:xx:xx --
    * SW0 button pressed
    * Device is connecting using WPS Push Button option
    * Wi-Fi request WPS
    * SSID : xxxxxx, authtyp : x pw : xxxxxxxx
    * Request Wi-Fi connect
    * Wi-Fi connected
    * Wi-Fi IP is xxx.xxx.xxx.xxx
    *
  8. To test WPS PIN method, Use case 2 in main function.
  9. Configure below code in the main.h for WPS PIN number and WPS push button feature.
    * #define WPS_PIN_NUMBER "12345670"
    *
  10. Enter WPS PIN number in the AP setup menu and start the AP. ( For more information, please refer to AP product documentation )
  11. Run the application. The WINC1500 will be connected to the AP automatically without security information.
    * -- WINC1500 security connection with Wi-Fi Protected Setup(WPS) example --
    * -- Compiled: xxx xx xxxx xx:xx:xx --
    * Wi-Fi request WPS
    * SSID : xxxxxx, authtyp : x pw : xxxxxxxx
    * Request Wi-Fi connect
    * Wi-Fi connected
    * Wi-Fi IP is xxx.xxx.xxx.xxx
    *

Compilation Information

This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.

Contact Information

For further information, visit Microchip.