Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Defines

     Specifies the macros and defines used by the Wlan APIs.

Modules

 DebugDefines
 

Macros

#define DEFAULT_CONF_AR_INITIALIZER   { 5, 1, TX_RATE_AUTO, TX_RATE_AUTO, 10, 5, 3 }
 
#define M2M_802_1X_MSCHAP2_FLAG   0x01
 
#define M2M_802_1X_PREPEND_DOMAIN_FLAG   0x40
 
#define M2M_802_1X_TLS_CLIENT_CERTIFICATE   1
 
#define M2M_802_1X_TLS_FLAG   0x02
 
#define M2M_802_1X_UNENCRYPTED_USERNAME_FLAG   0x80
 
#define M2M_AP_CMD_BASE   70
 
#define M2M_AUTH_1X_CERT_LEN_MAX   1584
 
#define M2M_AUTH_1X_PASSWORD_LEN_MAX   256
 
#define M2M_AUTH_1X_PRIVATEKEY_LEN_MAX   256
 
#define M2M_AUTH_1X_USER_LEN_MAX   100
 
#define M2M_BUFFER_MAX_SIZE   (1600UL - 4)
 
#define M2M_CONFIG_CMD_BASE   1
 
#define M2M_CRED_ENCRYPT_FLAG   0x02
 
#define M2M_CRED_IS_ENCRYPTED_FLAG   0x20
 
#define M2M_CRED_IS_STORED_FLAG   0x10
 
#define M2M_CRED_STORE_FLAG   0x01
 
#define M2M_CRYPTO_CMD_BASE   1
 
#define M2M_CUST_IE_LEN_MAX   252
 
#define M2M_DEVICE_NAME_MAX   48
 
#define M2M_ETHERNET_HDR_LEN   14
 
#define M2M_ETHERNET_HDR_OFFSET   34
 
#define M2M_FASTCONNECT_DEFAULT_RSSI_THRESH   (-45)
 
#define M2M_GEN_CMD_BASE   105
 
#define M2M_LISTEN_INTERVAL   1
 
#define M2M_MAC_ADDRES_LEN   6
 
#define M2M_MAX_GRP_NUM_REQ   (127)
 
#define M2M_MAX_PSK_LEN   65
 
#define M2M_MAX_SSID_LEN   33
 
#define M2M_MIN_PSK_LEN   9
 
#define M2M_NTP_MAX_SERVER_NAME_LENGTH   32
 
#define M2M_OTA_CMD_BASE   100
 
#define M2M_SCAN_DEFAULT_NUM_PROBE   (2)
 
#define M2M_SCAN_DEFAULT_NUM_SLOTS   (2)
 
#define M2M_SCAN_DEFAULT_PASSIVE_SLOT_TIME   (300)
 
#define M2M_SCAN_DEFAULT_SLOT_TIME   (30)
 
#define M2M_SERVER_CMD_BASE   100
 
#define M2M_SHA256_CONTEXT_BUFF_LEN   (128)
 
#define M2M_STA_CMD_BASE   40
 
#define M2M_WIFI_CONN_BSSID_FLAG   0x01
 
#define MAX_HIDDEN_SITES   4
 
#define PSK_CALC_LEN   40
 
#define PWR_DEFAULT   PWR_HIGH
 
#define TLS_CERTS_CHUNKED_SIG_VALUE   0x6ec8
 
#define TLS_CRL_DATA_MAX_LEN   64
 
#define TLS_CRL_MAX_ENTRIES   10
 
#define TLS_CRL_TYPE_CERT_HASH   1
 
#define TLS_CRL_TYPE_NONE   0
 
#define TLS_FILE_NAME_MAX   48
 
#define TLS_SRV_SEC_MAX_FILES   8
 
#define TLS_SRV_SEC_START_PATTERN_LEN   8
 
#define WEP_104_KEY_SIZE   ((uint8)13)
 
#define WEP_104_KEY_STRING_SIZE   ((uint8)26)
 
#define WEP_40_KEY_SIZE   ((uint8)5)
 
#define WEP_40_KEY_STRING_SIZE   ((uint8)10)
 
#define WEP_KEY_MAX_INDEX   ((uint8)4)
 
#define WLAN_11B_RATES_INITIALIZER
 
#define WLAN_11BG_RATES_ASC_INITIALIZER
 
#define WLAN_11BGN_RATES_ASC_INITIALIZER
 
#define WLAN_11G_RATES_INITIALIZER
 
#define WLAN_11N_RATES_INITIALIZER
 

#define DEFAULT_CONF_AR_INITIALIZER   { 5, 1, TX_RATE_AUTO, TX_RATE_AUTO, 10, 5, 3 }
#define M2M_802_1X_MSCHAP2_FLAG   0x01

Flag to indicate 802.1x MsChapV2 credentials: domain/user-name/password.

Referenced by m2m_wifi_connect_1x_mschap2().

#define M2M_802_1X_PREPEND_DOMAIN_FLAG   0x40

Flag to indicate that the 802.1x domain name should be prepended to the user-name: "Domain\Username". If the flag is not set then domain name is appended to the user-name: "Username@Domain". (Note that the '@' or '\' must be included in the domain name.)

Referenced by m2m_wifi_connect_1x_mschap2(), and m2m_wifi_connect_1x_tls().

#define M2M_802_1X_TLS_CLIENT_CERTIFICATE   1

Info type used in tstrM2mWifiAuthInfoHdr to indicate Enterprise TLS client certificate.

Referenced by m2m_wifi_connect_1x_tls().

#define M2M_802_1X_TLS_FLAG   0x02

Flag to indicate 802.1x TLS credentials: domain/user-name/private-key/certificate.

Referenced by m2m_wifi_connect_1x_tls().

#define M2M_802_1X_UNENCRYPTED_USERNAME_FLAG   0x80

Flag to indicate that the 802.1x user-name should be sent (unencrypted) in the initial EAP identity response. Intended for use with EAP-TLS only.

Referenced by m2m_wifi_connect_1x_mschap2(), and m2m_wifi_connect_1x_tls().

#define M2M_AP_CMD_BASE   70

The base value of all the Access Point mode host commands opcodes.

#define M2M_AUTH_1X_CERT_LEN_MAX   1584

The maximum length (in bytes) of certificate for authentication with Enterprise TLS methods.

Referenced by m2m_wifi_connect_1x_tls().

#define M2M_AUTH_1X_PASSWORD_LEN_MAX   256

The maximum length (in ASCII characters) of password for authentication with Enterprise MSCHAPv2 methods.

Referenced by m2m_wifi_connect_1x_mschap2().

#define M2M_AUTH_1X_PRIVATEKEY_LEN_MAX   256

The maximum length (in bytes) of private key modulus for authentication with Enterprise TLS methods. Private key exponent must be the same length as modulus, pre-padded with 0s if necessary.

Referenced by m2m_wifi_connect_1x_tls().

#define M2M_AUTH_1X_USER_LEN_MAX   100

The maximum length (in ASCII characters) of domain name + username (including '@' or '\') for authentication with Enterprise methods.

Referenced by m2m_wifi_connect_1x_mschap2(), and m2m_wifi_connect_1x_tls().

#define M2M_BUFFER_MAX_SIZE   (1600UL - 4)

Maximum size for the shared packet buffer.

#define M2M_CONFIG_CMD_BASE   1

The base value of all the host configuration commands opcodes.

#define M2M_CRED_ENCRYPT_FLAG   0x02

Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials should be encrypted when stored in WINC flash.

Referenced by m2m_wifi_connect_prepare_msg().

#define M2M_CRED_IS_ENCRYPTED_FLAG   0x20

Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials are encrypted in WINC flash. May only be set by WINC firmware.

#define M2M_CRED_IS_STORED_FLAG   0x10

Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials are stored in WINC flash. May only be set by WINC firmware.

#define M2M_CRED_STORE_FLAG   0x01

Flag used in tstrM2mConnCredHdr to indicate that Wi-Fi connection credentials should be stored in WINC flash.

Referenced by m2m_wifi_connect_prepare_msg().

#define M2M_CRYPTO_CMD_BASE   1

The base value of all the crypto mode host commands opcodes. The crypto Have special group so can extended from 1-M2M_MAX_GRP_NUM_REQ

#define M2M_CUST_IE_LEN_MAX   252

The maximum size of IE (Information Element).

Referenced by m2m_wifi_set_cust_InfoElement().

#define M2M_DEVICE_NAME_MAX   48

Maximum Size for the device name including the NULL termination.

Referenced by m2m_wifi_set_device_name().

#define M2M_ETHERNET_HDR_LEN   14

Length of the Ethernet header in bytes.

Referenced by m2m_wifi_send_ethernet_pkt().

#define M2M_ETHERNET_HDR_OFFSET   34

The offset of the Ethernet header within the WLAN Tx Buffer.

Referenced by m2m_wifi_send_ethernet_pkt().

#define M2M_FASTCONNECT_DEFAULT_RSSI_THRESH   (-45)

The default threshold RSSI for fast reconnection to an AP.

#define M2M_GEN_CMD_BASE   105

The base value of additional host wifi command opcodes. Usage restrictions (eg STA mode only) should always be made clear at the API layer in any case.

#define M2M_LISTEN_INTERVAL   1

The STA uses the Listen Interval parameter to indicate to the AP how many beacon intervals it shall sleep before it retrieves the queued frames from the AP.

#define M2M_MAC_ADDRES_LEN   6

The size of the 802 MAC address.

Referenced by m2m_wifi_connect_prepare_msg().

#define M2M_MAX_GRP_NUM_REQ   (127)

max number of request in one group equal to 127 as the last bit reserved for config or data pkt

#define M2M_MAX_PSK_LEN   65

1 more than the WPA PSK length (in ASCII format). This matches the size of the WPA PSK/Passphrase buffer (max ASCII contents + 1-byte length field). Alternatively it matches the WPA PSK length (in ASCII format) + 1 byte NULL termination.

Referenced by m2m_validate_ap_parameters(), m2m_wifi_connect_psk(), and m2m_wifi_connect_sc().

#define M2M_MAX_SSID_LEN   33

1 more than the max SSID length. This matches the size of SSID buffers (max SSID length + 1-byte length field).

Referenced by m2m_validate_ap_parameters(), m2m_wifi_connect_prepare_msg(), m2m_wifi_connect_sc(), m2m_wifi_delete_sc(), and m2m_wifi_request_scan_ssid_list().

#define M2M_MIN_PSK_LEN   9

1 more than the minimum WPA PSK Passphrase length. It matches the minimum WPA PSK Passphrase length + 1 byte NULL termination.

Referenced by m2m_validate_ap_parameters().

#define M2M_NTP_MAX_SERVER_NAME_LENGTH   32

Maximum NTP server name length

Referenced by m2m_wifi_configure_sntp().

#define M2M_OTA_CMD_BASE   100

The base value of all the OTA mode host commands opcodes. The OTA Have special group so can extended from 1-M2M_MAX_GRP_NUM_REQ

#define M2M_SCAN_DEFAULT_NUM_PROBE   (2)

The default number of probes per scan slot.

Referenced by m2m_validate_scan_options().

#define M2M_SCAN_DEFAULT_NUM_SLOTS   (2)

The default number of scan slots used by the WINC board.

#define M2M_SCAN_DEFAULT_PASSIVE_SLOT_TIME   (300)

The passive scan slot default duration in ms.

#define M2M_SCAN_DEFAULT_SLOT_TIME   (30)

The default duration in miliseconds of an active scan slot used by the WINC board.

#define M2M_SERVER_CMD_BASE   100

The base value of all the power save mode host commands codes.

#define M2M_SHA256_CONTEXT_BUFF_LEN   (128)

sha256 context size

#define M2M_STA_CMD_BASE   40

The base value of all the station mode host commands opcodes.

#define M2M_WIFI_CONN_BSSID_FLAG   0x01

Flag used in tstrM2mConnCredCmn to indicate that Wi-Fi connection must be restricted to an AP with a certain BSSID.

Referenced by m2m_wifi_connect_prepare_msg().

#define MAX_HIDDEN_SITES   4

max number of hidden SSID supported by scan request

Referenced by m2m_wifi_request_scan_ssid_list().

#define PSK_CALC_LEN   40

PSK is 32 bytes generated either:

  • from 64 ASCII characters
  • by SHA1 operations on up to 63 ASCII characters 40 byte array is required during SHA1 operations, so we define PSK_CALC_LEN as 40.
#define PWR_DEFAULT   PWR_HIGH
#define TLS_CERTS_CHUNKED_SIG_VALUE   0x6ec8
#define TLS_CRL_DATA_MAX_LEN   64
#define TLS_CRL_MAX_ENTRIES   10
#define TLS_CRL_TYPE_CERT_HASH   1
#define TLS_CRL_TYPE_NONE   0
#define TLS_FILE_NAME_MAX   48

Maximum length for each TLS certificate file name including null terminator.

#define TLS_SRV_SEC_MAX_FILES   8

Maximum number of certificates allowed in TLS_SRV section.

#define TLS_SRV_SEC_START_PATTERN_LEN   8

Length of certificate struct start pattern.

#define WEP_104_KEY_SIZE   ((uint8)13)

The size in bytes of a 104-bit wep key.

#define WEP_104_KEY_STRING_SIZE   ((uint8)26)

The string length of a 104-bit wep key.

Referenced by m2m_validate_ap_parameters(), and m2m_wifi_connect_wep().

#define WEP_40_KEY_SIZE   ((uint8)5)

The size in bytes of a 40-bit wep key.

#define WEP_40_KEY_STRING_SIZE   ((uint8)10)

The string length of a 40-bit wep key.

Referenced by m2m_validate_ap_parameters(), and m2m_wifi_connect_wep().

#define WEP_KEY_MAX_INDEX   ((uint8)4)

WEP key index is in the range 1 to 4 inclusive. (This is decremented to result in an index in the range 0 to 3 on air.)

Referenced by m2m_validate_ap_parameters(), and m2m_wifi_connect_wep().

#define WLAN_11B_RATES_INITIALIZER
Value:
{ \
}
Definition: m2m_types.h:2787
Definition: m2m_types.h:2785
Definition: m2m_types.h:2786
Definition: m2m_types.h:2784
#define WLAN_11BG_RATES_ASC_INITIALIZER
Value:
{ \
}
Definition: m2m_types.h:2790
Definition: m2m_types.h:2791
Definition: m2m_types.h:2787
Definition: m2m_types.h:2789
Definition: m2m_types.h:2785
Definition: m2m_types.h:2794
Definition: m2m_types.h:2795
Definition: m2m_types.h:2793
Definition: m2m_types.h:2786
Definition: m2m_types.h:2788
Definition: m2m_types.h:2784
Definition: m2m_types.h:2792
#define WLAN_11BGN_RATES_ASC_INITIALIZER
Value:
{ \
}
Definition: m2m_types.h:2790
Definition: m2m_types.h:2791
Definition: m2m_types.h:2787
Definition: m2m_types.h:2789
Definition: m2m_types.h:2785
Definition: m2m_types.h:2794
Definition: m2m_types.h:2799
Definition: m2m_types.h:2798
Definition: m2m_types.h:2803
Definition: m2m_types.h:2800
Definition: m2m_types.h:2795
Definition: m2m_types.h:2793
Definition: m2m_types.h:2786
Definition: m2m_types.h:2802
Definition: m2m_types.h:2788
Definition: m2m_types.h:2796
Definition: m2m_types.h:2797
Definition: m2m_types.h:2784
Definition: m2m_types.h:2792
Definition: m2m_types.h:2801
#define WLAN_11G_RATES_INITIALIZER
Value:
{ \
}
Definition: m2m_types.h:2790
Definition: m2m_types.h:2791
Definition: m2m_types.h:2789
Definition: m2m_types.h:2794
Definition: m2m_types.h:2795
Definition: m2m_types.h:2793
Definition: m2m_types.h:2788
Definition: m2m_types.h:2792
#define WLAN_11N_RATES_INITIALIZER
Value:
{ \
}
Definition: m2m_types.h:2799
Definition: m2m_types.h:2798
Definition: m2m_types.h:2803
Definition: m2m_types.h:2800
Definition: m2m_types.h:2802
Definition: m2m_types.h:2796
Definition: m2m_types.h:2797
Definition: m2m_types.h:2801