SAM D21 AWS MAIN configuration.
AWS IoT specific configuration file.
Copyright (c) 2017-2019 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | AWS_IOT_CERTIFICATE_FILENAME " " |
#define | AWS_IOT_MQTT_CLIENT_ID "SAMD21_MQTT" |
#define | AWS_IOT_MQTT_HOST "AGOO5J5NTHNQB.iot.us-west-2.amazonaws.com" |
#define | AWS_IOT_MQTT_MAX_RECONNECT_WAIT_INTERVAL 8000 |
Maximum time interval after which exponential back-off will stop attempting to reconnect. More... | |
#define | AWS_IOT_MQTT_MIN_RECONNECT_WAIT_INTERVAL 1000 |
Minimum time before the First reconnect attempt is made as part of the exponential back-off algorithm. More... | |
#define | AWS_IOT_MQTT_NUM_SUBSCRIBE_HANDLERS 5 |
Maximum number of topic filters the MQTT client can handle at any given time. This should be increased appropriately when using Thing Shadow. More... | |
#define | AWS_IOT_MQTT_PORT 443 |
#define | AWS_IOT_MQTT_RX_BUF_LEN 512 |
Any message that comes into the device should be less than this buffer size. If a received message is bigger than this buffer size the message will be dropped. More... | |
#define | AWS_IOT_MQTT_TX_BUF_LEN 512 |
Any time a message is sent out through the MQTT layer. The message is copied into this buffer anytime a publish is done. This will also be used in the case of Thing Shadow. More... | |
#define | AWS_IOT_MY_THING_NAME "SAMD21_MQTT" |
#define | AWS_IOT_PRIVATE_KEY_FILENAME " " |
#define | AWS_IOT_ROOT_CA_FILENAME " " |
#define | MAX_ACKS_TO_COMEIN_AT_ANY_GIVEN_TIME 10 |
At Any given time we will wait for this many responses. This will correlate to the rate at which the shadow actions are requested. More... | |
#define | MAX_JSON_TOKEN_EXPECTED 120 |
These are the max tokens that are expected to be in the Shadow JSON document. Include the metadata that gets published. More... | |
#define | MAX_SHADOW_TOPIC_LENGTH_BYTES MAX_SHADOW_TOPIC_LENGTH_WITHOUT_THINGNAME + MAX_SIZE_OF_THING_NAME |
This size includes the length of topic with Thing Name. More... | |
#define | MAX_SHADOW_TOPIC_LENGTH_WITHOUT_THINGNAME 60 |
All shadow actions have to be published or subscribed to a topic which is of the format $aws/things/{thingName}/shadow/update/accepted. This refers to the size of the topic without the Thing Name. More... | |
#define | MAX_SIZE_CLIENT_ID_WITH_SEQUENCE MAX_SIZE_OF_UNIQUE_CLIENT_ID_BYTES + 10 |
This is size of the extra sequence number that will be appended to the Unique client Id. More... | |
#define | MAX_SIZE_CLIENT_TOKEN_CLIENT_SEQUENCE MAX_SIZE_CLIENT_ID_WITH_SEQUENCE + 20 |
This is size of the total clientToken key and value pair in the JSON. More... | |
#define | MAX_SIZE_OF_THING_NAME 20 |
The Thing Name should not be bigger than this value. Modify this if the Thing Name needs to be bigger. More... | |
#define | MAX_SIZE_OF_UNIQUE_CLIENT_ID_BYTES 80 |
Maximum size of the Unique Client Id. For More info on the Client Id refer Acknowledgments. More... | |
#define | MAX_THINGNAME_HANDLED_AT_ANY_GIVEN_TIME 10 |
We could perform shadow action on any Thing Name and this is maximum Thing Names we can act on at any given time. More... | |
#define | SHADOW_MAX_SIZE_OF_RX_BUFFER AWS_IOT_MQTT_RX_BUF_LEN+1 |
Maximum size of the SHADOW buffer to store the received Shadow message. More... | |
#define AWS_IOT_CERTIFICATE_FILENAME " " |
#define AWS_IOT_MQTT_CLIENT_ID "SAMD21_MQTT" |
#define AWS_IOT_MQTT_HOST "AGOO5J5NTHNQB.iot.us-west-2.amazonaws.com" |
#define AWS_IOT_MQTT_MAX_RECONNECT_WAIT_INTERVAL 8000 |
Maximum time interval after which exponential back-off will stop attempting to reconnect.
#define AWS_IOT_MQTT_MIN_RECONNECT_WAIT_INTERVAL 1000 |
Minimum time before the First reconnect attempt is made as part of the exponential back-off algorithm.
#define AWS_IOT_MQTT_NUM_SUBSCRIBE_HANDLERS 5 |
Maximum number of topic filters the MQTT client can handle at any given time. This should be increased appropriately when using Thing Shadow.
#define AWS_IOT_MQTT_PORT 443 |
#define AWS_IOT_MQTT_RX_BUF_LEN 512 |
Any message that comes into the device should be less than this buffer size. If a received message is bigger than this buffer size the message will be dropped.
Referenced by aws_iot_mqtt_connect().
#define AWS_IOT_MQTT_TX_BUF_LEN 512 |
Any time a message is sent out through the MQTT layer. The message is copied into this buffer anytime a publish is done. This will also be used in the case of Thing Shadow.
Referenced by aws_iot_mqtt_connect().
#define AWS_IOT_MY_THING_NAME "SAMD21_MQTT" |
#define AWS_IOT_PRIVATE_KEY_FILENAME " " |
#define AWS_IOT_ROOT_CA_FILENAME " " |
#define MAX_ACKS_TO_COMEIN_AT_ANY_GIVEN_TIME 10 |
At Any given time we will wait for this many responses. This will correlate to the rate at which the shadow actions are requested.
Referenced by AckStatusCallback(), getNextFreeIndexOfAckWaitList(), HandleExpiredResponseCallbacks(), and initializeRecords().
#define MAX_JSON_TOKEN_EXPECTED 120 |
These are the max tokens that are expected to be in the Shadow JSON document. Include the metadata that gets published.
Referenced by initDeltaTokens(), and registerJsonTokenOnDelta().
#define MAX_SHADOW_TOPIC_LENGTH_BYTES MAX_SHADOW_TOPIC_LENGTH_WITHOUT_THINGNAME + MAX_SIZE_OF_THING_NAME |
This size includes the length of topic with Thing Name.
Referenced by incrementSubscriptionCnt(), isSubscriptionPresent(), publishToShadowAction(), registerJsonTokenOnDelta(), and unsubscribeFromAcceptedAndRejected().
#define MAX_SHADOW_TOPIC_LENGTH_WITHOUT_THINGNAME 60 |
All shadow actions have to be published or subscribed to a topic which is of the format $aws/things/{thingName}/shadow/update/accepted. This refers to the size of the topic without the Thing Name.
#define MAX_SIZE_CLIENT_ID_WITH_SEQUENCE MAX_SIZE_OF_UNIQUE_CLIENT_ID_BYTES + 10 |
This is size of the extra sequence number that will be appended to the Unique client Id.
#define MAX_SIZE_CLIENT_TOKEN_CLIENT_SEQUENCE MAX_SIZE_CLIENT_ID_WITH_SEQUENCE + 20 |
This is size of the total clientToken key and value pair in the JSON.
Referenced by AckStatusCallback(), addToAckWaitList(), aws_iot_shadow_delete(), aws_iot_shadow_get(), and iot_shadow_action().
#define MAX_SIZE_OF_THING_NAME 20 |
The Thing Name should not be bigger than this value. Modify this if the Thing Name needs to be bigger.
Referenced by addToAckWaitList(), and aws_iot_shadow_connect().
#define MAX_SIZE_OF_UNIQUE_CLIENT_ID_BYTES 80 |
Maximum size of the Unique Client Id. For More info on the Client Id refer Acknowledgments.
Referenced by aws_iot_shadow_connect().
#define MAX_THINGNAME_HANDLED_AT_ANY_GIVEN_TIME 10 |
We could perform shadow action on any Thing Name and this is maximum Thing Names we can act on at any given time.
#define SHADOW_MAX_SIZE_OF_RX_BUFFER AWS_IOT_MQTT_RX_BUF_LEN+1 |
Maximum size of the SHADOW buffer to store the received Shadow message.
Referenced by AckStatusCallback(), and shadow_delta_callback().