Typedefs | |
typedef void(* | tpfAppResolveCb )(uint8 *pu8DomainName, uint32 u32ServerIP) |
DNS resolution callback function. Applications requiring DNS resolution should register their callback through this function by calling registerSocketCallback. The following callback is triggered in response to an asynchronous call to the gethostbyname function (DNS Resolution callback). More... | |
typedef void(* | tpfAppSocketCb )(SOCKET sock, uint8 u8Msg, void *pvMsg) |
The main socket application callback function. Applications register their main socket application callback through this function by calling registerSocketCallback. In response to events received, the following callback function is called to handle the corresponding asynchronous function called. Example: bind, connect,...etc. More... | |
typedef void(* | tpfPingCb )(uint32 u32IPAddr, uint32 u32RTT, uint8 u8ErrorCode) |
PING Callback. More... | |
tpfAppResolveCb |
DNS resolution callback function.
Applications requiring DNS resolution should register their callback through this function by calling registerSocketCallback. The following callback is triggered in response to an asynchronous call to the gethostbyname function (DNS Resolution callback).
[in] | pu8DomainName | Domain name of the host. |
[in] | u32ServerIP | Server IPv4 address encoded in Network byte order format. If it is Zero, then the DNS resolution failed. |
tpfAppSocketCb |
The main socket application callback function. Applications register their main socket application callback through this function by calling registerSocketCallback. In response to events received, the following callback function is called to handle the corresponding asynchronous function called. Example: bind, connect,...etc.
[in] | sock | Socket ID for the callback. |
The socket callback function is called whenever a new event is received in response to socket operations.
[in] | u8Msg | Socket event type. Possible values are: |
[in] | pvMsg | Pointer to message structure. Existing types are: |
tpfPingCb |
PING Callback.
The function delivers the ping statistics for the sent ping triggered by calling @ref m2m_ping_req.
[in] | u32IPAddr | Destination IP. |
[in] | u32RTT | Round Trip Time. |
[in] | u8ErrorCode | Ping error code. It may be one of:
|