Microchip® Advanced Software Framework

tstrM2mWifiAuthInfoHdr Struct Reference

Generic Wi-Fi authentication information to be sent in a separate HIF message of type M2M_WIFI_IND_CONN_PARAM (preceding M2M_WIFI_REQ_CONN).

#include <m2m_types.h>

Data Fields

uint8 au8Info []
 
uint8 au8Rsv [3]
 
uint16 u16InfoLen
 
uint16 u16InfoPos
 
uint8 u8Type
 

uint8 tstrM2mWifiAuthInfoHdr::au8Info[]

Placeholder for info.

uint8 tstrM2mWifiAuthInfoHdr::au8Rsv[3]

Reserved for future use. Set to 0.

uint16 tstrM2mWifiAuthInfoHdr::u16InfoLen

Info length (not including this header).

Referenced by m2m_wifi_connect_1x_tls().

uint16 tstrM2mWifiAuthInfoHdr::u16InfoPos

Information about positioning of the Info. The interpretation depends on u8Type.

Referenced by m2m_wifi_connect_1x_tls().

uint8 tstrM2mWifiAuthInfoHdr::u8Type