Introduction
This empty project is a placeholder for the tools to use to perform the following actions:
- WINC3400 firmware update
- WINC3400 root certificate update
It can be used with the following hardware:
- the SAMD21 Xplained Pro.
- the WINC3400 (must be connected to EXT1).
For a more information about WINC3400 update please refer to the following document available under the doc folder:
- Atmel-Firmware-Update-Procedure-for-WINC-Module-using-a-SAM-Xplained-Pro.pdf
Main Files
- samd21_xplained_pro_firmware_update.bat : script to perform firmware update.
Contact Information
For further information, visit Microchip.