Microchip® Advanced Software Framework

hr_sensor.h File Reference

Heart Rate Sensor Profile declarations.

Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.

Macros

#define ACTIVITY_BRISK_WALKING   (2)
 
#define ACTIVITY_FAST_RUNNING   (4)
 
#define ACTIVITY_NORMAL   (0)
 Activities of user. More...
 
#define ACTIVITY_RUNNING   (3)
 
#define ACTIVITY_WALKING   (1)
 
#define ADV_DATA_LEN   (18)
 ADV_DATA_LEN. More...
 
#define ADV_TYPE_LEN   (0x01)
 ADV_TYPE_LEN. More...
 
#define APP_HRS_ADV_TIMEOUT   (1000)
 APP_HRS_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x3FFF in seconds, 0x0000 disables time-out. More...
 
#define APP_HRS_FAST_ADV   (100)
 
#define DEFAULT_ACTIVITY   (0xFF)
 
#define END_OF_LAST_ACTIVITY   (200)
 
#define ENERGY_EXP_BRISK_WALKING   (20)
 
#define ENERGY_EXP_FAST_RUNNING   (60)
 
#define ENERGY_EXP_NORMAL   (3)
 energy expended for various activities More...
 
#define ENERGY_EXP_RUNNING   (40)
 
#define ENERGY_EXP_WALKING   (10)
 
#define ENERGY_EXPENDED_FIELD_PRESENT   (0x1 << 3)
 ENERGY_EXPENDED_FIELD_PRESENT represents energy expended inclusion. More...
 
#define ENERGY_RESET   (0)
 
#define HEART_RATE_INCREMENT_VALUE   (1)
 Heart rate increment value. More...
 
#define HEART_RATE_MAX_BRISK_WALK   (110)
 
#define HEART_RATE_MAX_FAST_RUNNING   (151)
 
#define HEART_RATE_MAX_NORM   (70)
 
#define HEART_RATE_MAX_RUNNING   (130)
 
#define HEART_RATE_MAX_WALKING   (90)
 
#define HEART_RATE_MIN_BRISK_WALK   (91)
 
#define HEART_RATE_MIN_FAST_RUNNING   (130)
 
#define HEART_RATE_MIN_NORM   (50)
 Heart Rate maximum and minimum values for various activities. More...
 
#define HEART_RATE_MIN_RUNNING   (111)
 
#define HEART_RATE_MIN_WALKING   (71)
 
#define HR_CHAR_VALUE_LEN   (10)
 The maximum length of the hr measurement characteristic data. More...
 
#define HR_VALUE_FORMAT_UINT16   (0x1 << 0)
 HR_VALUE_FORMAT_UINT16 the bit to represent hr value sent is 16 bit. More...
 
#define HRS_ADV_DATA_NAME_DATA   ("ATMEL-HRT")
 
#define HRS_ADV_DATA_NAME_LEN   (9)
 HRS_ADV_DATA_NAME_LEN the length of the device name. More...
 
#define HRS_ADV_DATA_NAME_TYPE   (0x09)
 HRS_ADV_DATA_NAME_TYPE the gap ad data type. More...
 
#define HRS_ADV_DATA_UUID_LEN   (2)
 HRS_ADV_DATA_UUID_LEN the size of HRS service uuid. More...
 
#define HRS_ADV_DATA_UUID_TYPE   (0x03)
 HRS_ADV_DATA_UUID_TYPE the total sizeof HRS service uuid. More...
 
#define NOTIFICATION_INTERVAL   (1000)
 Notification interval to determine the frequency of notifications. More...
 
#define RR_INTERVAL_VALUE_PRESENT   (0x1 << 4)
 RR_INTERVAL_VALUE_PRESENT represents the rr value inclusion. More...
 
#define RR_VALUE_MAX   (1000)
 RR interval maximum and minimum values for simulation of rr values. More...
 
#define RR_VALUE_MIN   (100)
 
#define SCAN_RESP_LEN   (10)
 scan_resp_len is the length of the scan response data More...
 
#define SENSOR_CONTACT_FTR_NOT_SPRTD_CONTACT_DTD   (0x3 << 1)
 SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info. More...
 
#define SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT   (0x1 << 2)
 SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info. More...
 
#define START_OF_FIRST_ACTIVITY   (0)
 time limit of last activity More...
 

Functions

void ble_heart_rate_handle_disconnect_event (at_ble_handle_t conn_handle)
 
void ble_heart_rate_handle_paired_event (at_ble_handle_t conn_handle)
 
void ble_heart_rate_profile_init (void)
 hr_sensor_init initializes and defines the services of the hr profile More...
 
at_ble_status_t ble_heart_rate_start_advertise (void)
 
void heart_rate_send_notification (uint8_t *char_data, uint8_t length)
 

Variables

uint8_t activity
 
uint16_t energy_expended_val
 
uint8_t energy_inclusion
 
uint16_t energy_incrementor
 
uint16_t heart_rate_value
 
uint8_t hr_max_value
 
uint8_t hr_min_value
 
uint8_t inc_changer
 
uint8_t notification_flag
 
uint8_t prev_activity
 
uint8_t second_counter
 
uint8_t time_operator
 
bool volatile timer_cb_done
 

#define ACTIVITY_BRISK_WALKING   (2)
#define ACTIVITY_FAST_RUNNING   (4)
#define ACTIVITY_NORMAL   (0)
#define ACTIVITY_RUNNING   (3)
#define ACTIVITY_WALKING   (1)
#define ADV_DATA_LEN   (18)

ADV_DATA_LEN.

#define ADV_TYPE_LEN   (0x01)

ADV_TYPE_LEN.

Referenced by ble_heart_rate_start_advertise().

#define APP_HRS_ADV_TIMEOUT   (1000)

APP_HRS_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x3FFF in seconds, 0x0000 disables time-out.

Referenced by ble_heart_rate_start_advertise().

#define APP_HRS_FAST_ADV   (100)
#define DEFAULT_ACTIVITY   (0xFF)
#define END_OF_LAST_ACTIVITY   (200)
#define ENERGY_EXP_BRISK_WALKING   (20)
#define ENERGY_EXP_FAST_RUNNING   (60)
#define ENERGY_EXP_NORMAL   (3)

energy expended for various activities

Referenced by ble_heart_rate_handle_disconnect_event(), and ble_heart_rate_value_init().

#define ENERGY_EXP_RUNNING   (40)
#define ENERGY_EXP_WALKING   (10)
#define ENERGY_EXPENDED_FIELD_PRESENT   (0x1 << 3)

ENERGY_EXPENDED_FIELD_PRESENT represents energy expended inclusion.

Referenced by ble_heart_rate_process().

#define ENERGY_RESET   (0)

Referenced by ble_heart_rate_process().

#define HEART_RATE_INCREMENT_VALUE   (1)

Heart rate increment value.

Referenced by ble_heart_rate_process().

#define HEART_RATE_MAX_BRISK_WALK   (110)
#define HEART_RATE_MAX_FAST_RUNNING   (151)
#define HEART_RATE_MAX_NORM   (70)
#define HEART_RATE_MAX_RUNNING   (130)
#define HEART_RATE_MAX_WALKING   (90)
#define HEART_RATE_MIN_BRISK_WALK   (91)
#define HEART_RATE_MIN_FAST_RUNNING   (130)
#define HEART_RATE_MIN_NORM   (50)

Heart Rate maximum and minimum values for various activities.

Referenced by ble_heart_rate_value_init().

#define HEART_RATE_MIN_RUNNING   (111)
#define HEART_RATE_MIN_WALKING   (71)
#define HR_CHAR_VALUE_LEN   (10)

The maximum length of the hr measurement characteristic data.

Referenced by ble_heart_rate_process().

#define HR_VALUE_FORMAT_UINT16   (0x1 << 0)

HR_VALUE_FORMAT_UINT16 the bit to represent hr value sent is 16 bit.

#define HRS_ADV_DATA_NAME_DATA   ("ATMEL-HRT")
#define HRS_ADV_DATA_NAME_LEN   (9)

HRS_ADV_DATA_NAME_LEN the length of the device name.

Referenced by ble_heart_rate_start_advertise().

#define HRS_ADV_DATA_NAME_TYPE   (0x09)

HRS_ADV_DATA_NAME_TYPE the gap ad data type.

Referenced by ble_heart_rate_start_advertise().

#define HRS_ADV_DATA_UUID_LEN   (2)

HRS_ADV_DATA_UUID_LEN the size of HRS service uuid.

Referenced by ble_heart_rate_start_advertise().

#define HRS_ADV_DATA_UUID_TYPE   (0x03)

HRS_ADV_DATA_UUID_TYPE the total sizeof HRS service uuid.

Referenced by ble_heart_rate_start_advertise().

#define NOTIFICATION_INTERVAL   (1000)

Notification interval to determine the frequency of notifications.

Referenced by ble_heart_rate_handle_paired_event().

#define RR_INTERVAL_VALUE_PRESENT   (0x1 << 4)

RR_INTERVAL_VALUE_PRESENT represents the rr value inclusion.

Referenced by ble_heart_rate_process().

#define RR_VALUE_MAX   (1000)

RR interval maximum and minimum values for simulation of rr values.

Referenced by ble_heart_rate_process().

#define RR_VALUE_MIN   (100)

Referenced by ble_heart_rate_process().

#define SCAN_RESP_LEN   (10)

scan_resp_len is the length of the scan response data

Referenced by ble_heart_rate_start_advertise().

#define SENSOR_CONTACT_FTR_NOT_SPRTD_CONTACT_DTD   (0x3 << 1)

SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info.

#define SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT   (0x1 << 2)

SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info.

#define START_OF_FIRST_ACTIVITY   (0)

time limit of last activity

Referenced by ble_heart_rate_handle_timer_event().

void heart_rate_send_notification ( uint8_t *  char_data,
uint8_t  length 
)

uint8_t activity
uint16_t energy_expended_val

to count the energy expended

Referenced by ble_heart_rate_handle_disconnect_event(), and ble_heart_rate_process().

uint8_t energy_inclusion

To check for including the energy in hr measurement

Referenced by ble_heart_rate_handle_disconnect_event(), and ble_heart_rate_process().

uint16_t energy_incrementor

energy incrementor for various heart rate values

Referenced by ble_heart_rate_process(), and ble_heart_rate_value_init().

uint16_t heart_rate_value

to count the heart rate value

Referenced by ble_heart_rate_process(), and ble_heart_rate_value_init().

uint8_t hr_max_value

the maximum heart rate value

Referenced by ble_heart_rate_value_init().

uint8_t hr_min_value

the minimum heart rate value

Referenced by ble_heart_rate_value_init().

uint8_t inc_changer

increment operator to change heart rate

Referenced by ble_heart_rate_process(), and ble_heart_rate_value_init().

uint8_t notification_flag

flag to show notification

Referenced by ble_heart_rate_handle_timer_event().

uint8_t prev_activity
uint8_t time_operator

operator to change the seconds

Referenced by ble_heart_rate_handle_timer_event().