Microchip® Advanced Software Framework

tstrSystemTime Struct Reference

This struct contains the system time.

#include <m2m_types.h>

Data Fields

uint8 __PAD__ [__PADDING_tstrSystemTime_]
 
uint16 u16Year
 
uint8 u8Day
 
uint8 u8Hour
 
uint8 u8Minute
 
uint8 u8Month
 
uint8 u8Second
 

uint8 tstrSystemTime::__PAD__[__PADDING_tstrSystemTime_]

Structure padding.

uint16 tstrSystemTime::u16Year

Year

uint8 tstrSystemTime::u8Day

Day

uint8 tstrSystemTime::u8Hour

Hour

uint8 tstrSystemTime::u8Minute

Minutes

uint8 tstrSystemTime::u8Month

Month

uint8 tstrSystemTime::u8Second

Seconds