WINC3400 IoT Application Interface Internal Types.
Copyright (c) 2017-2021 Microchip Technology Inc. and its subsidiaries.
|
struct | tstrM2MAPConfig |
| This structure holds the configuration parameters for the AP mode. It should be set by the application when it requests to enable the AP operation mode. The AP mode currently supports only OPEN and WEP security. More...
|
|
struct | tstrM2MAPConfigExt |
| AP Configuration Extension. More...
|
|
struct | tstrM2MAPModeConfig |
| AP Configuration. More...
|
|
struct | tstrM2mBatteryVoltage |
| This struct stores the battery voltage. More...
|
|
struct | tstrM2mBleApiMsg |
| This struct contains a BLE message. More...
|
|
struct | tstrM2MBLEInfo |
| BLE Result. More...
|
|
struct | tstrM2mClientState |
| This struct contains the information for the PS Client state. More...
|
|
struct | tstrM2mConnCredCmn |
| Wi-Fi Connect Credentials Common section. More...
|
|
struct | tstrM2mConnCredHdr |
| Wi-Fi Connect Credentials Header. More...
|
|
struct | tstrM2MConnInfo |
| This struct contains the connection information. More...
|
|
struct | tstrM2MDefaultConnResp |
| This struct contains the response error of m2m_default_connect. More...
|
|
struct | tstrM2MDeviceNameConfig |
| This struct contains the Device Name of the WINC. It is used mainly for Wi-Fi Direct device discovery and WPS device information. More...
|
|
struct | tstrM2mEnableLogs |
| This struct stores logging information. More...
|
|
struct | tstrM2MGainTable |
| This struct contains the information of the gain table index from flash to be used. More...
|
|
struct | tstrM2MGainTableRsp |
| This struct contains response when the firmware has failed to configure the gains from flash. More...
|
|
struct | tstrM2MGenericResp |
| Generic success/error response. More...
|
|
struct | tstrM2MIPConfig |
| This struct contains the static IP configuration. More...
|
|
struct | tstrM2mIpRsvdPkt |
| This struct contains the size and data offset for the received packet. More...
|
|
struct | tstrM2mLsnInt |
| This struct contains the Listen Interval. It is the value of the Wi-Fi StA Listen Interval when power save is enabled. It is given in units of Beacon period. It is the number of Beacon periods the WINC can sleep before it wakes up to receive data buffered for it in the AP. More...
|
|
struct | tstrM2MMulticastMac |
| This struct contains the information from the Multicast filter. More...
|
|
struct | tstrM2MP2PConnect |
| This struct contains the Listen Channel for P2P connect. More...
|
|
struct | tstrM2MProvisionInfo |
| This struct contains the provisioning information obtained from the HTTP Provisioning server. More...
|
|
struct | tstrM2MProvisionModeConfig |
| This struct contains the provisioning mode configuration. More...
|
|
struct | tstrM2mPsType |
| This struct contains the Power Save configuration. More...
|
|
struct | tstrM2mPwrMode |
|
struct | tstrM2mReqScanResult |
| The Wi-Fi Scan results list is stored in firmware. This struct contains the index by which the application can request a certain scan result. More...
|
|
struct | tstrM2MScan |
| This struct contains the Wi-Fi scan request. More...
|
|
struct | tstrM2mScanDone |
| This struct contains the Wi-Fi scan result. More...
|
|
struct | tstrM2MScanOption |
| This struct contains the configuration options for Wi-Fi scan. More...
|
|
struct | tstrM2MScanRegion |
| This struct contains the Wi-Fi information for the channel regions. More...
|
|
struct | tstrM2Mservercmd |
| This struct contains the information for the PS Server command. More...
|
|
struct | tstrM2mServerInit |
| This struct contains the information for the PS Server initialization. More...
|
|
struct | tstrM2mSetMacAddress |
| This struct contains the MAC address to be used. The WINC loads the mac address from the efuse by default to the WINC configuration memory, however, the application can overwrite the configuration memory with the mac address indicated from the Host. More...
|
|
struct | tstrM2mSlpReqTime |
| This struct contains the sleep time for the Power Save request. More...
|
|
struct | tstrM2MSNTPConfig |
| SNTP Client Configuration. More...
|
|
struct | tstrM2MStopScanOption |
| This struct holds additional configuration options for Wi-Fi scan. More...
|
|
struct | tstrM2mTxPwrLevel |
| This struct stores the Tx Power levels. More...
|
|
struct | tstrM2mWifi1xHdr |
| Wi-Fi Authentication 802.1x header for parameters. The parameters (Domain, UserName, PrivateKey/Password) are appended to this structure. More...
|
|
struct | tstrM2mWifiApId |
| Specify an access point (by SSID) More...
|
|
struct | tstrM2mWifiAuthInfoHdr |
| Generic Wi-Fi authentication information to be sent in a separate HIF message of type M2M_WIFI_IND_CONN_PARAM (preceding M2M_WIFI_REQ_CONN). More...
|
|
struct | tstrM2mWifiConnectLegacy_1_2 |
| Wi-Fi Connect Request IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages. For general usage, this structure is replaced by tstrM2mWifiConnHdr. More...
|
|
struct | tstrM2mWifiConnHdr |
| Wi-Fi Connect Request (new format) for use with M2M_WIFI_REQ_CONN. This structure is sent across the HIF along with the relevant auth details. One of: tstrM2mWifiPsk tstrM2mWifiWep tstrM2mWifi1xHdr If further authentication details need to be sent (such as client certificate for 1x TLS), they are sent with header tstrM2mWifiAuthInfoHdr in a preceding HIF message of type M2M_WIFI_IND_CONN_PARAM. More...
|
|
struct | tstrM2MWifiMonitorModeCtrl |
| This struct contains the Wi-Fi Monitor Mode Filter. It sets the filtering criteria for WLAN packets when monitoring mode is enabled. The received packets matching the filtering parameters, are passed directly to the application. More...
|
|
struct | tstrM2mWifiPsk |
|
struct | tstrM2mWiFiRoaming |
| Roaming related information. More...
|
|
struct | tstrM2MWifiRxPacketInfo |
| This struct contains the Wi-Fi RX Frame Header. The M2M application has the ability to allow Wi-Fi monitoring mode for receiving all Wi-Fi Raw frames matching a well defined filtering criteria. When a target Wi-Fi packet is received, the header information are extracted and assigned in this structure. More...
|
|
struct | tstrM2mWifiscanResult |
| This struct contains the information corresponding to an AP in the scan result list identified by its order (index) in the list. More...
|
|
struct | tstrM2MWifiSecInfoLegacy_1_2 |
| Authentication credentials to connect to a Wi-Fi network. IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages. More...
|
|
struct | tstrM2mWifiStateChanged |
| This struct contains the Wi-Fi connection state. More...
|
|
struct | tstrM2MWifiTxPacketInfo |
| This struct contains the Wi-Fi TX Packet Info. The M2M Application has the ability to compose raw Wi-Fi frames (under the application responsibility). When transmitting a Wi-Fi packet, the application must supply the firmware with this structure for sending the target frame. More...
|
|
struct | tstrM2mWifiWep |
| WEP security key header. More...
|
|
struct | tstrM2mWifiWepParamsLegacy_1_2 |
| WEP security key parameters. IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages. More...
|
|
struct | tstrM2MWPSConnect |
| This struct stores the WPS configuration parameters. More...
|
|
struct | tstrM2MWPSInfo |
| WPS Result. More...
|
|
struct | tstrOtaControlSec |
| Control Section Structure. The Control Section is used to define the working image and the validity of the roll-back image and its offset, also both firmware versions are kept in this structure. More...
|
|
struct | tstrOtaInitHdr |
| This struct contains the OTA image header. More...
|
|
struct | tstrOtaUpdateInfo |
| This struct contains the OTA update information. More...
|
|
struct | tstrOtaUpdateStatusResp |
| This struct contains the OTA update status. More...
|
|
struct | tstrPrng |
| M2M Request PRNG. More...
|
|
struct | tstrRootCertEcdsaKeyInfo |
| Info about a ECDSA public key. More...
|
|
struct | tstrRootCertEntryHeader |
| Header of a root certificate entry in flash. More...
|
|
struct | tstrRootCertFlashHeader |
| Header of the root certificate flash storage area. More...
|
|
struct | tstrRootCertPubKeyInfo |
| Info about the public key contained in a root certificate. More...
|
|
struct | tstrRootCertRsaKeyInfo |
| Info about a RSA public key. More...
|
|
struct | tstrSslSetActiveCsList |
|
struct | tstrSystemTime |
| This struct contains the system time. More...
|
|
struct | tstrTlsSrvChunkHdr |
|
struct | tstrTlsSrvSecFileEntry |
| This struct contains a TLS certificate. More...
|
|
struct | tstrTlsSrvSecHdr |
| This struct contains a set of TLS certificates. More...
|
|
union | tuniM2MWifiAuthLegacy_1_2 |
| Wi-Fi Security Parameters for all supported security modes. IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages. More...
|
|
|
enum | tenuM2mApCmd {
M2M_WIFI_REQ_ENABLE_AP_LEGACY = M2M_AP_CMD_BASE,
M2M_WIFI_REQ_DISABLE_AP,
M2M_WIFI_REQ_ENABLE_AP,
M2M_WIFI_MAX_AP_ALL
} |
| This enum contains WINC commands while in AP mode. More...
|
|
enum | tenuM2mConfigCmd {
M2M_WIFI_REQ_RESTART = M2M_CONFIG_CMD_BASE,
M2M_WIFI_REQ_SET_MAC_ADDRESS,
M2M_WIFI_REQ_CURRENT_RSSI,
M2M_WIFI_RESP_CURRENT_RSSI,
M2M_WIFI_REQ_RESTRICT_BLE,
M2M_WIFI_REQ_UNRESTRICT_BLE,
M2M_WIFI_REQ_GET_CONN_INFO,
M2M_WIFI_RESP_CONN_INFO,
M2M_WIFI_REQ_SET_DEVICE_NAME,
M2M_WIFI_REQ_START_PROVISION_MODE_LEGACY,
M2M_WIFI_RESP_PROVISION_INFO,
M2M_WIFI_REQ_STOP_PROVISION_MODE,
M2M_WIFI_REQ_SET_SYS_TIME,
M2M_WIFI_REQ_ENABLE_SNTP_CLIENT,
M2M_WIFI_REQ_DISABLE_SNTP_CLIENT,
M2M_WIFI_RESP_MEMORY_RECOVER,
M2M_WIFI_REQ_CUST_INFO_ELEMENT,
M2M_WIFI_REQ_SCAN,
M2M_WIFI_RESP_SCAN_DONE,
M2M_WIFI_REQ_SCAN_RESULT,
M2M_WIFI_RESP_SCAN_RESULT,
M2M_WIFI_REQ_SET_SCAN_OPTION,
M2M_WIFI_REQ_SET_SCAN_REGION,
M2M_WIFI_REQ_SET_POWER_PROFILE,
M2M_WIFI_REQ_SET_TX_POWER,
M2M_WIFI_REQ_SET_BATTERY_VOLTAGE,
M2M_WIFI_REQ_SET_ENABLE_LOGS,
M2M_WIFI_REQ_GET_SYS_TIME,
M2M_WIFI_RESP_GET_SYS_TIME,
M2M_WIFI_REQ_SEND_ETHERNET_PACKET,
M2M_WIFI_RESP_ETHERNET_RX_PACKET,
M2M_WIFI_REQ_SET_MAC_MCAST,
M2M_WIFI_REQ_BLE_API_SEND,
M2M_WIFI_RESP_BLE_API_RECV,
M2M_WIFI_REQ_SET_GAIN_TABLE,
M2M_WIFI_RESP_SET_GAIN_TABLE,
M2M_WIFI_REQ_PASSIVE_SCAN,
M2M_WIFI_REQ_CONFIG_SNTP,
M2M_WIFI_REQ_START_PROVISION_MODE,
M2M_WIFI_MAX_CONFIG_ALL
} |
| This enum contains host commands used to configure the WINC board. More...
|
|
enum | tenuM2mConnChangedErrcode {
M2M_ERR_SCAN_FAIL = ((uint8)1),
M2M_ERR_JOIN_FAIL,
M2M_ERR_AUTH_FAIL,
M2M_ERR_ASSOC_FAIL,
M2M_ERR_CONN_INPROGRESS
} |
|
enum | tenuM2mConnState {
M2M_WIFI_DISCONNECTED = 0,
M2M_WIFI_CONNECTED,
M2M_WIFI_ROAMED,
M2M_WIFI_UNDEF = 0xff
} |
| This enum contains all the Wi-Fi connection states. More...
|
|
enum | tenuM2mDefaultConnErrcode {
M2M_DEFAULT_CONN_INPROGRESS = ((sint8)-23),
M2M_DEFAULT_CONN_FAIL,
M2M_DEFAULT_CONN_SCAN_MISMATCH,
M2M_DEFAULT_CONN_EMPTY_LIST
} |
|
enum | tenuM2mGenCmd {
M2M_WIFI_REQRSP_DELETE_APID = M2M_GEN_CMD_BASE,
M2M_WIFI_REQ_ROAMING,
M2M_WIFI_REQ_SCAN_SSID_LIST,
M2M_WIFI_REQ_SET_STOP_SCAN_OPTION,
M2M_WIFI_MAX_GEN_ALL
} |
| This enum contains additional WINC commands (overflow of previous enums). More...
|
|
enum | tenuM2mIpCmd {
M2M_IP_REQ_STATIC_IP_CONF = ((uint8) 10),
M2M_IP_REQ_ENABLE_DHCP,
M2M_IP_REQ_DISABLE_DHCP
} |
| This enum contains all the WINC commands related to IP. More...
|
|
enum | tenuM2mOtaCmd {
M2M_OTA_REQ_NOTIF_SET_URL = M2M_OTA_CMD_BASE,
M2M_OTA_REQ_NOTIF_CHECK_FOR_UPDATE,
M2M_OTA_REQ_NOTIF_SCHED,
M2M_OTA_REQ_START_UPDATE,
M2M_OTA_REQ_SWITCH_FIRMWARE,
M2M_OTA_REQ_ROLLBACK,
M2M_OTA_REQ_ABORT,
M2M_OTA_RESP_NOTIF_UPDATE_INFO,
M2M_OTA_RESP_UPDATE_STATUS,
M2M_OTA_REQ_TEST,
M2M_OTA_MAX_ALL
} |
| This enum contains all the WINC commands used for OTA operation. More...
|
|
enum | tenuM2mP2pCmd {
M2M_WIFI_REQ_P2P_INT_CONNECT = M2M_P2P_CMD_BASE,
M2M_WIFI_REQ_ENABLE_P2P,
M2M_WIFI_REQ_DISABLE_P2P,
M2M_WIFI_REQ_P2P_REPOST,
M2M_WIFI_MAX_P2P_ALL
} |
| This enum contains WINC commands while in P2P mode. More...
|
|
enum | tenuM2mPwrMode {
PWR_AUTO = ((uint8) 1),
PWR_LOW1,
PWR_LOW2,
PWR_HIGH
} |
|
enum | tenuM2mReqGroup {
M2M_REQ_GROUP_MAIN = 0,
M2M_REQ_GROUP_WIFI,
M2M_REQ_GROUP_IP,
M2M_REQ_GROUP_HIF,
M2M_REQ_GROUP_OTA,
M2M_REQ_GROUP_SSL,
M2M_REQ_GROUP_SIGMA,
M2M_REQ_GROUP_INTERNAL
} |
|
enum | tenuM2mReqpkt {
M2M_REQ_CONFIG_PKT,
M2M_REQ_DATA_PKT = 0x80
} |
|
enum | tenuM2mScanCh {
M2M_WIFI_CH_1 = ((uint8) 1),
M2M_WIFI_CH_2,
M2M_WIFI_CH_3,
M2M_WIFI_CH_4,
M2M_WIFI_CH_5,
M2M_WIFI_CH_6,
M2M_WIFI_CH_7,
M2M_WIFI_CH_8,
M2M_WIFI_CH_9,
M2M_WIFI_CH_10,
M2M_WIFI_CH_11,
M2M_WIFI_CH_12,
M2M_WIFI_CH_13,
M2M_WIFI_CH_14,
M2M_WIFI_CH_ALL = ((uint8) 255)
} |
| This enum contains all the Wi-Fi RF channels. More...
|
|
enum | tenuM2mScanRegion {
REG_CH_1 = ((uint16) 1 << 0),
REG_CH_2 = ((uint16) 1 << 1),
REG_CH_3 = ((uint16) 1 << 2),
REG_CH_4 = ((uint16) 1 << 3),
REG_CH_5 = ((uint16) 1 << 4),
REG_CH_6 = ((uint16) 1 << 5),
REG_CH_7 = ((uint16) 1 << 6),
REG_CH_8 = ((uint16) 1 << 7),
REG_CH_9 = ((uint16) 1 << 8),
REG_CH_10 = ((uint16) 1 << 9),
REG_CH_11 = ((uint16) 1 << 10),
REG_CH_12 = ((uint16) 1 << 11),
REG_CH_13 = ((uint16) 1 << 12),
REG_CH_14 = ((uint16) 1 << 13),
REG_CH_ALL = ((uint16) 0x3FFF),
NORTH_AMERICA = ((uint16) 0x7FF),
EUROPE = ((uint16) 0x1FFF),
ASIA = ((uint16) 0x3FFF)
} |
| This enum contains all the Wi-Fi channel regions. More...
|
|
enum | tenuM2mSecType {
M2M_WIFI_SEC_INVALID = 0,
M2M_WIFI_SEC_OPEN,
M2M_WIFI_SEC_WPA_PSK,
M2M_WIFI_SEC_WEP,
M2M_WIFI_SEC_802_1X,
M2M_WIFI_NUM_AUTH_TYPES
} |
| This enum contains all the supported Wi-Fi security types. More...
|
|
enum | tenuM2mServerCmd {
M2M_WIFI_REQ_CLIENT_CTRL = M2M_SERVER_CMD_BASE,
M2M_WIFI_RESP_CLIENT_INFO,
M2M_WIFI_REQ_SERVER_INIT,
M2M_WIFI_MAX_SERVER_ALL
} |
| These commands are currently not supported. More...
|
|
enum | tenuM2mSetGainsErrcode {
M2M_ERR_GAIN_TABLE_INVALID = ((sint8)-10),
M2M_ERR_READ_GAIN_TABLE
} |
|
enum | tenuM2mSigmaCmd {
M2M_SIGMA_ENABLE = ((uint8) 3),
M2M_SIGMA_TA_START,
M2M_SIGMA_TA_STATS,
M2M_SIGMA_TA_RECEIVE_STOP,
M2M_SIGMA_ICMP_ARP,
M2M_SIGMA_ICMP_RX,
M2M_SIGMA_ICMP_TX,
M2M_SIGMA_UDP_TX,
M2M_SIGMA_UDP_TX_DEFER,
M2M_SIGMA_SECURITY_POLICY,
M2M_SIGMA_SET_SYSTIME
} |
| This enum contains all the WINC commands related to Sigma. More...
|
|
enum | tenuM2mSsidMode {
SSID_MODE_VISIBLE = 0,
SSID_MODE_HIDDEN
} |
|
enum | tenuM2mSslCmd {
M2M_SSL_REQ_CERT_VERIF,
M2M_SSL_REQ_ECC,
M2M_SSL_RESP_ECC,
M2M_SSL_RSV,
M2M_SSL_REQ_WRITE_OWN_CERTS,
M2M_SSL_REQ_SET_CS_LIST,
M2M_SSL_RESP_SET_CS_LIST,
M2M_SSL_RESP_WRITE_OWN_CERTS
} |
| This enum contains WINC commands related to TLS handshake. More...
|
|
enum | tenuM2mStaCmd {
M2M_WIFI_REQ_CONNECT = M2M_STA_CMD_BASE,
M2M_WIFI_REQ_DEFAULT_CONNECT,
M2M_WIFI_RESP_DEFAULT_CONNECT,
M2M_WIFI_REQ_DISCONNECT,
M2M_WIFI_RESP_CON_STATE_CHANGED,
M2M_WIFI_REQ_SLEEP,
M2M_WIFI_REQ_WPS_SCAN,
M2M_WIFI_REQ_WPS,
M2M_WIFI_REQ_START_WPS,
M2M_WIFI_REQ_DISABLE_WPS,
M2M_WIFI_REQ_DHCP_CONF,
M2M_WIFI_RESP_IP_CONFIGURED,
M2M_WIFI_RESP_IP_CONFLICT,
M2M_WIFI_REQ_ENABLE_MONITORING,
M2M_WIFI_REQ_DISABLE_MONITORING,
M2M_WIFI_RESP_WIFI_RX_PACKET,
M2M_WIFI_REQ_SEND_WIFI_PACKET,
M2M_WIFI_REQ_LSN_INT,
M2M_WIFI_REQ_DOZE,
M2M_WIFI_REQ_GET_PRNG,
M2M_WIFI_RESP_GET_PRNG,
M2M_WIFI_REQ_CONN,
M2M_WIFI_IND_CONN_PARAM,
M2M_WIFI_MAX_STA_ALL
} |
| This enum contains WINC commands while in Station mode. More...
|
|
enum | tenuM2mTxPwrLevel {
TX_PWR_HIGH = ((uint8) 1),
TX_PWR_MED,
TX_PWR_LOW
} |
|
enum | tenuM2mWepKeyIndex {
M2M_WIFI_WEP_KEY_INDEX_1 = ((uint8) 1),
M2M_WIFI_WEP_KEY_INDEX_2,
M2M_WIFI_WEP_KEY_INDEX_3,
M2M_WIFI_WEP_KEY_INDEX_4
} |
|
enum | tenuM2mWifiMode {
M2M_WIFI_MODE_NORMAL = ((uint8) 1),
M2M_WIFI_MODE_CONFIG,
M2M_WIFI_MODE_ETHERNET,
M2M_WIFI_MODE_MAX
} |
| This enum contains all the supported Wi-Fi Operation Modes. More...
|
|
enum | tenuOtaError {
OTA_SUCCESS = (0),
OTA_ERR_WORKING_IMAGE_LOAD_FAIL = ((sint8) -1),
OTA_ERR_INVALID_CONTROL_SEC = ((sint8) -2),
M2M_ERR_OTA_SWITCH_FAIL = ((sint8) -3),
M2M_ERR_OTA_START_UPDATE_FAIL = ((sint8) -4),
M2M_ERR_OTA_ROLLBACK_FAIL = ((sint8) -5),
M2M_ERR_OTA_INVALID_FLASH_SIZE = ((sint8) -6),
M2M_ERR_OTA_INVALID_ARG = ((sint8) -7),
M2M_ERR_OTA_INPROGRESS = ((sint8) -8)
} |
| OTA Error codes. More...
|
|
enum | tenuOtaUpdateStatus {
OTA_STATUS_SUCCESS = 0,
OTA_STATUS_FAIL = 1,
OTA_STATUS_INVALID_ARG = 2,
OTA_STATUS_INVALID_RB_IMAGE = 3,
OTA_STATUS_INVALID_FLASH_SIZE = 4,
OTA_STATUS_ALREADY_ENABLED = 5,
OTA_STATUS_UPDATE_INPROGRESS = 6,
OTA_STATUS_IMAGE_VERIF_FAILED = 7,
OTA_STATUS_CONNECTION_ERROR = 8,
OTA_STATUS_SERVER_ERROR = 9,
OTA_STATUS_ABORTED = 10
} |
| This struct contains the OTA return status. More...
|
|
enum | tenuOtaUpdateStatusType {
DL_STATUS = 1,
SW_STATUS = 2,
RB_STATUS = 3,
AB_STATUS = 4
} |
| This struct contains the OTA update status type. More...
|
|
enum | tenuPowerSaveModes {
M2M_NO_PS,
M2M_PS_AUTOMATIC,
M2M_PS_H_AUTOMATIC,
M2M_PS_DEEP_AUTOMATIC,
M2M_PS_MANUAL
} |
| This enum contains all the supported Wi-Fi Power Save modes. More...
|
|
enum | tenuRootCertPubKeyType {
ROOT_CERT_PUBKEY_RSA = 1,
ROOT_CERT_PUBKEY_ECDSA = 2
} |
| This enum contains the supported public key types for TLS root certificates. More...
|
|
enum | tenuSNTPUseDHCP {
SNTP_DISABLE_DHCP = 0,
SNTP_ENABLE_DHCP = 1
} |
| Use NTP server provided by the DHCP server. More...
|
|
enum | tenuTlsFlashStatus {
TLS_FLASH_OK,
TLS_FLASH_OK_NO_CHANGE,
TLS_FLASH_ERR_CORRUPT,
TLS_FLASH_ERR_NO_CHANGE,
TLS_FLASH_ERR_UNKNOWN
} |
|
enum | tenuWPSTrigger {
WPS_PIN_TRIGGER = 0,
WPS_PBC_TRIGGER = 4
} |
| This enum contains the WPS triggering methods. More...
|
|