Microchip® Advanced Software Framework

tstrM2MDefaultConnResp Struct Reference

This struct contains the response error of m2m_default_connect.

See Also
M2M_DEFAULT_CONN_SCAN_MISMATCH M2M_DEFAULT_CONN_EMPTY_LIST

#include <m2m_types.h>

Data Fields

uint8 __PAD24__ [3]
 
sint8 s8ErrorCode
 

uint8 tstrM2MDefaultConnResp::__PAD24__[3]
sint8 tstrM2MDefaultConnResp::s8ErrorCode

Default connect error code. possible values are:

  • M2M_DEFAULT_CONN_EMPTY_LIST
  • M2M_DEFAULT_CONN_SCAN_MISMATCH