Typedefs | |
typedef signed short | sint16 |
Range of values between -32768 to 32767. More... | |
typedef signed long | sint32 |
Range of values between -2147483648 to 2147483647. More... | |
typedef signed char | sint8 |
Range of values between -128 to 127. More... | |
typedef void(* | tpfNmBspIsr )(void) |
Pointer to function. Used as a data type of ISR function registered by nm_bsp_register_isr. More... | |
typedef unsigned short | uint16 |
Range of values between 0 to 65535. More... | |
typedef unsigned long | uint32 |
Range of values between 0 to 4294967295. More... | |
typedef unsigned char | uint8 |
Range of values between 0 to 255. More... | |
signed short sint16 |
Range of values between -32768 to 32767.
signed long sint32 |
Range of values between -2147483648 to 2147483647.
signed char sint8 |
Range of values between -128 to 127.
Pointer to function.
Used as a data type of ISR function registered by nm_bsp_register_isr.
unsigned short uint16 |
Range of values between 0 to 65535.
unsigned long uint32 |
Range of values between 0 to 4294967295.
unsigned char uint8 |
Range of values between 0 to 255.