Generic data structure used for all lwIP network interfaces.
The following fields should be filled in by the initialization function for the device driver: hwaddr_len, hwaddr[], mtu, flags
#include <netif.h>
Data Fields | |
struct autoip * | autoip |
the AutoIP client state information for this netif More... | |
struct dhcp * | dhcp |
the DHCP client state information for this netif More... | |
u8_t | flags |
flags (see NETIF_FLAG_ above) More... | |
ip_addr_t | gw |
u8_t | hwaddr [NETIF_MAX_HWADDR_LEN] |
link level hardware address of this interface More... | |
u8_t | hwaddr_len |
number of bytes used in hwaddr More... | |
netif_input_fn | input |
This function is called by the network device driver to pass a packet up the TCP/IP stack. More... | |
ip6_addr_t | ip6_addr [LWIP_IPV6_NUM_ADDRESSES] |
Array of IPv6 addresses for this netif. More... | |
u8_t | ip6_addr_state [LWIP_IPV6_NUM_ADDRESSES] |
The state of each IPv6 address (Tentative, Preferred, etc). More... | |
u8_t | ip6_autoconfig_enabled |
is this netif enabled for IPv6 autoconfiguration More... | |
ip_addr_t | ip_addr |
IP address configuration in network byte order. More... | |
netif_linkoutput_fn | linkoutput |
This function is called by the ARP module when it wants to send a packet on the interface. More... | |
netif_mld_mac_filter_fn | mld_mac_filter |
This function could be called to add or delete an entry in the IPv6 multicast filter table of the ethernet MAC. More... | |
u16_t | mtu |
maximum transfer unit (in bytes) More... | |
char | name [2] |
descriptive abbreviation More... | |
ip_addr_t | netmask |
struct netif * | next |
pointer to next in linked list More... | |
u8_t | num |
number of this interface More... | |
netif_output_fn | output |
This function is called by the IP module when it wants to send a packet on the interface. More... | |
netif_output_ip6_fn | output_ip6 |
This function is called by the IPv6 module when it wants to send a packet on the interface. More... | |
u8_t | rs_count |
Number of Router Solicitation messages that remain to be sent. More... | |
void * | state |
This field can be set by the device driver and could point to state information for the device. More... | |
netif_status_callback_fn | status_callback |
This function is called when the netif state is set to up or down. More... | |
struct autoip* netif::autoip |
the AutoIP client state information for this netif
Referenced by autoip_arp_announce(), autoip_arp_probe(), autoip_arp_reply(), autoip_bind(), autoip_create_addr(), autoip_handle_arp_conflict(), autoip_network_changed(), autoip_restart(), autoip_set_struct(), autoip_start(), autoip_start_probing(), autoip_stop(), autoip_tmr(), ip_input(), netif_add(), and netif_set_link_up().
struct dhcp* netif::dhcp |
the DHCP client state information for this netif
Referenced by dhcp_arp_reply(), dhcp_bind(), dhcp_check(), dhcp_cleanup(), dhcp_coarse_tmr(), dhcp_decline(), dhcp_discover(), dhcp_fine_tmr(), dhcp_handle_ack(), dhcp_handle_nak(), dhcp_handle_offer(), dhcp_inform(), dhcp_network_changed(), dhcp_rebind(), dhcp_reboot(), dhcp_recv(), dhcp_release(), dhcp_renew(), dhcp_select(), dhcp_set_struct(), dhcp_start(), dhcp_stop(), dhcp_t1_timeout(), dhcp_t2_timeout(), dhcp_timeout(), netif_add(), netif_set_link_up(), and udp_input().
u8_t netif::flags |
flags (see NETIF_FLAG_ above)
Referenced by dhcp_start(), dhcp_stop(), ethernet_input(), ip4_addr_isbroadcast(), ip_input(), nd6_tmr(), netif_add(), netif_remove(), netif_set_down(), netif_set_link_down(), netif_set_link_up(), netif_set_up(), tcpip_input(), and winc_netif_low_level_init().
ip_addr_t netif::gw |
Referenced by autoip_start(), etharp_output(), netif_add(), and netif_set_gw().
u8_t netif::hwaddr[NETIF_MAX_HWADDR_LEN] |
link level hardware address of this interface
Referenced by autoip_arp_announce(), autoip_arp_probe(), autoip_arp_reply(), dhcp_create_msg(), dhcp_recv(), etharp_output(), etharp_output_to_arp_index(), etharp_query(), etharp_request(), etharp_update_arp_entry(), ethernet_input(), ethip6_output(), nd6_send_na(), nd6_send_ns(), nd6_send_rs(), netif_create_ip6_linklocal_address(), and winc_netif_low_level_init().
u8_t netif::hwaddr_len |
number of bytes used in hwaddr
Referenced by dhcp_create_msg(), dhcp_recv(), etharp_arp_input(), etharp_raw(), etharp_send_ip(), etharp_update_arp_entry(), ethip6_send(), nd6_input(), nd6_send_na(), nd6_send_ns(), nd6_send_rs(), netif_create_ip6_linklocal_address(), and winc_netif_low_level_init().
netif_input_fn netif::input |
This function is called by the network device driver to pass a packet up the TCP/IP stack.
Referenced by netif_add(), and winc_netif_rx_callback().
ip6_addr_t netif::ip6_addr[LWIP_IPV6_NUM_ADDRESSES] |
Array of IPv6 addresses for this netif.
Referenced by nd6_tmr(), netif_add(), and netif_create_ip6_linklocal_address().
u8_t netif::ip6_addr_state[LWIP_IPV6_NUM_ADDRESSES] |
The state of each IPv6 address (Tentative, Preferred, etc).
Referenced by nd6_tmr(), and netif_create_ip6_linklocal_address().
u8_t netif::ip6_autoconfig_enabled |
is this netif enabled for IPv6 autoconfiguration
Referenced by nd6_tmr(), and netif_add().
ip_addr_t netif::ip_addr |
IP address configuration in network byte order.
Referenced by autoip_start(), dhcp_create_msg(), etharp_arp_input(), etharp_output(), etharp_request(), ip4_addr_isbroadcast(), ip_input(), ip_route(), netif_add(), netif_set_ipaddr(), status_callback(), udp_connect(), and udp_input().
netif_linkoutput_fn netif::linkoutput |
This function is called by the ARP module when it wants to send a packet on the interface.
This function outputs the pbuf as-is on the link medium.
Referenced by etharp_arp_input(), etharp_raw(), etharp_send_ip(), ethip6_send(), and winc_netif_init().
netif_mld_mac_filter_fn netif::mld_mac_filter |
This function could be called to add or delete an entry in the IPv6 multicast filter table of the ethernet MAC.
Referenced by mld6_joingroup(), mld6_leavegroup(), mld6_stop(), netif_add(), and winc_netif_init().
u16_t netif::mtu |
maximum transfer unit (in bytes)
Referenced by dhcp_start(), ip6_output_if_src(), ip_frag(), nd6_get_destination_mtu(), nd6_get_next_hop_entry(), nd6_input(), tcp_eff_send_mss_impl(), and winc_netif_low_level_init().
char netif::name[2] |
descriptive abbreviation
Referenced by autoip_bind(), autoip_start(), dhcp_bind(), dhcp_check(), dhcp_handle_nak(), dhcp_handle_offer(), dhcp_select(), dhcp_start(), ip6_input(), ip6_output_if_src(), ip_input(), netif_add(), netif_find(), netif_set_default(), netif_set_gw(), netif_set_ipaddr(), netif_set_netmask(), and winc_netif_init().
ip_addr_t netif::netmask |
Referenced by autoip_start(), etharp_output(), ip4_addr_isbroadcast(), ip_input(), ip_route(), netif_add(), netif_set_netmask(), and udp_input().
struct netif* netif::next |
pointer to next in linked list
Referenced by autoip_tmr(), dhcp_coarse_tmr(), dhcp_fine_tmr(), ip6_input(), ip6_route(), ip_input(), ip_route(), mld6_joingroup(), mld6_leavegroup(), nd6_tmr(), netif_add(), netif_find(), and netif_remove().
u8_t netif::num |
number of this interface
Referenced by autoip_bind(), autoip_start(), dhcp_bind(), dhcp_handle_nak(), dhcp_handle_offer(), dhcp_select(), dhcp_start(), ip6_output_if_src(), netif_add(), and netif_find().
netif_output_fn netif::output |
This function is called by the IP module when it wants to send a packet on the interface.
This function typically first resolves the hardware address, then sends the packet.
Referenced by ip_frag(), and winc_netif_init().
netif_output_ip6_fn netif::output_ip6 |
This function is called by the IPv6 module when it wants to send a packet on the interface.
This function typically first resolves the hardware address, then sends the packet.
Referenced by ip6_output_if_src(), netif_add(), and winc_netif_init().
u8_t netif::rs_count |
Number of Router Solicitation messages that remain to be sent.
Referenced by nd6_input(), nd6_tmr(), netif_add(), and netif_set_up().
void* netif::state |
This field can be set by the device driver and could point to state information for the device.
Referenced by etharp_cleanup_netif(), etharp_find_addr(), etharp_update_arp_entry(), nd6_tmr(), netif_add(), and winc_netif_init().
netif_status_callback_fn netif::status_callback |
This function is called when the netif state is set to up or down.
Referenced by netif_add(), and netif_set_status_callback().