WINC3400 (Wi-Fi + BLE) | |
Standard I/O (stdio) | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
Standard serial I/O (stdio) | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
BSP | Description of the BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) module. |
Data Types | |
Defines | |
Functions | Lists the available BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) APIs. |
Common | |
Defines | |
Functions | |
Flash | |
Enumeration/Typedefs | |
Functions | |
OTA | The WINC supports OTA (Over-The-Air) updates. |
Callbacks | Lists the different callbacks that can be used during OTA updates. |
Defines | Specifies the macros and defines used by the OTA APIs. |
Enumerations and Typedefs | Specifies the enums and Data Structures used by the OTA APIs. |
Functions | Lists the full set of available APIs to manage OTA updates and Host File Downloads. |
SSL | Provides a description of the SSL Layer. |
Callbacks | Provides detail on the available callbacks for the SSL Layer. |
Enumerations and Typedefs | Specifies the enums and Data Structures used by the SSL APIs. |
Functions | Provides detail on the available APIs for the SSL Layer. |
TLS Defines | |
TLS Socket Options | The following list of macros are used to define SSL Socket options |
TLS Cipher Suite IDs | The following list of macros defined the list of supported TLS Cipher suites |
Version | Describes the APIs for reading the version information of the WINC firmware. |
Defines | Specifies the macros and defines used by the version APIs. |
Functions | Lists the APIs for reading the version information of the WINC firmware. |
WLAN | |
Callbacks | Provides detail on the available callbacks for the Wlan APIs. |
Defines | Specifies the macros and defines used by the Wlan APIs. |
Enumerations and Typedefs | Specifies the enums and Data Structures used by the Wlan APIs. |
Functions | Here are listed all the functions that implement the Wlan APIs. |
Initialization | Here are listed all the functions that implement the Wlan Initialization APIs. |
Wlan Events | Here are listed all the functions that implement the Wlan Events APIs. |
Connection | Here are listed all the functions that implement the Wifi Connection APIs. |
Scanning | Here are listed all the functions that implement the Wifi Scanning APIs. |
Hot-Spot (Access-Point) | Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs. |
Bypass Mode | Here are listed all the functions that implement the Bypass Mode APIs. |
Roaming | Here are listed all the functions that implement the Wifi Roaming APIs. |
Power Save | Here are listed all the functions that implement the Power-Save APIs. |
Configuration | Here are listed all the functions that implement the Wlan Configuration APIs. |
System Time | Here are listed all the functions that implement the System Time APIs. |
Provisioning | Here are listed all the functions that implement the Wifi Provisioning APIs. |
Crypto | Here are listed all the functions that implement the Wifi Crypto APIs. |
BLE | Here are listed all the functions that implement the BLE APIs. |
Socket | BSD compatible socket interface between the host layer and the network protocol stacks in the firmware |
Defines | The following list of macros are used to define constants used throughout the socket layer, and SSL Socket options |
TCP/IP Defines | The following list of macros are used to define constants used throughout the socket layer |
TLS Defines | |
TLS Socket Options | The following list of macros are used to define SSL Socket options |
TLS Cipher Suite IDs | The following list of macros defined the list of supported TLS Cipher suites |
Byte Order | The following list of macros are used to convert between host representation and network byte order |
Error Codes | The following list of macros are used to define the possible error codes |
Enumeration/Typedefs | Specific Enumeration-typedefs used for socket operations |
Asynchronous Events | Specific Enumeration used for asynchronous operations |
Callbacks | |
Functions | The function performs the necessary initializations for the socket library through the following steps: |
SPI FLASH | |
Functions | |
SAM Port (PORT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing |
Compiler abstraction layer and code utilities | Compiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices |
Status Codes | |
Preprocessor - Macro Recursion | |
Preprocessor - Macro Repeat | |
Preprocessor - Stringize | |
Preprocessor - Token Paste | |
Global interrupt management | This is a driver for global enabling and disabling of interrupts |
Deprecated interrupt definitions | |
Atmel part identification macros | This collection of macros identify which series and families that the various Atmel parts belong to |
AVR UC3 parts | |
AVR XMEGA parts | |
megaAVR parts | |
SAM parts | |
SAM System Pin Multiplexer (SYSTEM PINMUX) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection |
SAM Serial Peripheral Interface (SERCOM SPI) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its SPI mode to transfer SPI data frames |
SAM System (SYSTEM) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation |
SAM System Clock Management (SYSTEM CLOCK) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions |
SAM System Interrupt (SYSTEM INTERRUPT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions |
Busy-Wait Delay Routines | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
SAM External Interrupt (EXTINT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of external interrupts generated by the physical device pins, including edge detection |
SAM Timer Counter for Control Applications (TCC) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the TCC module within the device, for waveform generation and timing operations |
Serial Interface (Serial) | See Quick start guide for Serial Interface service |
SAM Serial USART (SERCOM USART) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its USART mode to transfer or receive USART data frames |
Generic board support | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
SAM D21 Xplained Pro board | |
Features | Symbols that describe features and capabilities of the board |