This struct contains the MAC address to be used. The WINC loads the mac address from the efuse by default to the WINC configuration memory, however, the application can overwrite the configuration memory with the mac address indicated from the Host.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD16__ [2] |
uint8 | au8Mac [6] |
uint8 tstrM2mSetMacAddress::__PAD16__[2] |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2mSetMacAddress::au8Mac[6] |
MAC address
Referenced by m2m_wifi_set_mac_address().