This struct contains the information corresponding to an AP in the scan result list identified by its order (index) in the list.
#include <m2m_types.h>
Data Fields | |
uint8 | _PAD8_ |
uint8 | au8BSSID [6] |
uint8 | au8SSID [M2M_MAX_SSID_LEN] |
sint8 | s8rssi |
uint8 | u8AuthType |
uint8 | u8ch |
uint8 | u8index |
uint8 tstrM2mWifiscanResult::_PAD8_ |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2mWifiscanResult::au8BSSID[6] |
BSSID of the AP.
uint8 tstrM2mWifiscanResult::au8SSID[M2M_MAX_SSID_LEN] |
AP SSID.
Referenced by ble_prov_scan_result().
sint8 tstrM2mWifiscanResult::s8rssi |
AP signal strength.
Referenced by ble_prov_scan_result().
uint8 tstrM2mWifiscanResult::u8AuthType |
AP authentication type.
Referenced by ble_prov_scan_result().
uint8 tstrM2mWifiscanResult::u8ch |
AP RF channel.
uint8 tstrM2mWifiscanResult::u8index |
AP index in the scan result list.