Microchip® Advanced Software Framework

All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Modules
Here is a list of all modules:
[detail level 1234]
oWINC3400 (Wi-Fi + BLE)
oPower Management Controller (PMC)
oPeripheral Parallel Input/Output (PIO) Controller
oSerial Peripheral Interface (SPI)See Quickstart guide for SAM SPI driver
oUniversal Asynchronous Receiver Transceiver (UART)The Universal Asynchronous Receiver Transmitter features a two-pin UART that can be used for communication and trace purposes and offers an ideal medium for in-situ programming solutions
oUniversal Synchronous AsynchronousReceiver Transmitter (USART)
oStandard I/O (stdio)Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices
|\Standard serial I/O (stdio)Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices
oWatchdog Timer (WDT)Driver for the WDT (Watchdog Timer)
oBSP
Description of the BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) module.
|oData Types
|oDefines
|\Functions
    Lists the available BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) APIs.
oCommon
|oDefines
|\Functions
oFlash
|oEnumeration/Typedefs
|\Functions
oOTA
 The WINC supports OTA (Over-The-Air) updates.
|oCallbacks
     Lists the different callbacks that can be used during OTA updates.
|oDefines
     Specifies the macros and defines used by the OTA APIs.
|oEnumerations and Typedefs
     Specifies the enums and Data Structures used by the OTA APIs.
|\Functions
     Lists the full set of available APIs to manage OTA updates and Host File Downloads.
oSSL
Provides a description of the SSL Layer.
|oCallbacks
    Provides detail on the available callbacks for the SSL Layer.
|oEnumerations and Typedefs
    Specifies the enums and Data Structures used by the SSL APIs.
|oFunctions
    Provides detail on the available APIs for the SSL Layer.
|\TLS Defines
| oTLS Socket OptionsThe following list of macros are used to define SSL Socket options
| \TLS Cipher Suite IDsThe following list of macros defined the list of supported TLS Cipher suites
oVersion
Describes the APIs for reading the version information of the WINC firmware.
|oDefines
    Specifies the macros and defines used by the version APIs.
|\Functions
    Lists the APIs for reading the version information of the WINC firmware.
oWLAN
|oCallbacks
    Provides detail on the available callbacks for the Wlan APIs.
|oDefines
    Specifies the macros and defines used by the Wlan APIs.
|oEnumerations and Typedefs
    Specifies the enums and Data Structures used by the Wlan APIs.
|\Functions
    Here are listed all the functions that implement the Wlan APIs.
| oInitialization
        Here are listed all the functions that implement the Wlan Initialization APIs.
| oWlan Events
        Here are listed all the functions that implement the Wlan Events APIs.
| oConnection
        Here are listed all the functions that implement the Wifi Connection APIs.
| oScanning
        Here are listed all the functions that implement the Wifi Scanning APIs.
| oHot-Spot (Access-Point)
        Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs.
| oBypass Mode
        Here are listed all the functions that implement the Bypass Mode APIs.
| oRoaming
        Here are listed all the functions that implement the Wifi Roaming APIs.
| oPower Save
        Here are listed all the functions that implement the Power-Save APIs.
| oConfiguration
        Here are listed all the functions that implement the Wlan Configuration APIs.
| oSystem Time
        Here are listed all the functions that implement the System Time APIs.
| oProvisioning
        Here are listed all the functions that implement the Wifi Provisioning APIs.
| oCrypto
        Here are listed all the functions that implement the Wifi Crypto APIs.
| \BLE
        Here are listed all the functions that implement the BLE APIs.
oSocketBSD compatible socket interface between the host layer and the network protocol stacks in the firmware
|oDefinesThe following list of macros are used to define constants used throughout the socket layer, and SSL Socket options
||oTCP/IP DefinesThe following list of macros are used to define constants used throughout the socket layer
||\TLS Defines
|| oTLS Socket OptionsThe following list of macros are used to define SSL Socket options
|| \TLS Cipher Suite IDsThe following list of macros defined the list of supported TLS Cipher suites
|oByte OrderThe following list of macros are used to convert between host representation and network byte order
|oError CodesThe following list of macros are used to define the possible error codes
|oEnumeration/TypedefsSpecific Enumeration-typedefs used for socket operations
||\Asynchronous EventsSpecific Enumeration used for asynchronous operations
|oCallbacks
|\Functions
         The function performs the necessary initializations for the socket library through the following steps:
oSPI FLASH
|\Functions
oPower Manager (PM)This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service
oCompiler abstraction layer and code utilitiesCompiler abstraction layer and code utilities for AT91SAM
|oPreprocessor - Macro Repeat
|oPreprocessor - Stringize
|\Preprocessor - Token Paste
oGlobal interrupt managementThis is a driver for global enabling and disabling of interrupts
|\Deprecated interrupt definitions
oAtmel part identification macrosThis collection of macros identify which series and families that the various Atmel parts belong to
|oAVR UC3 parts
|oAVR XMEGA parts
|omegaAVR parts
|\SAM parts
oSAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the the Peripheral Direct Memory Access (DMA) Controller (PDC) module
oClock Management
|oGeneric Clock ManagementGeneric clocks are configurable clocks which run outside the system clock domain
|oOscillator ManagementThis group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators
|oPLL ManagementThis group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs
|\System Clock ManagementSee Quick Start Guide for the System Clock Management service (SAM4S)
oCommon IOPORT APISee Quick start guide for the common IOPORT service
oBusy-Wait Delay RoutinesThis module provides simple loop-based delay routines for those applications requiring a brief wait during execution
oSAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality
oSerial Interface (Serial)See Quick start guide for Serial Interface service
oUniversal Synchronous Asynchronous ReceiverTransmitter (USART)
oGeneric board supportThe generic board support module includes board-specific definitions and function prototypes, such as the board initialization function
|\SAM4S Xplained Pro board
| oConfigurationSymbols to use for configuring the board and its initialization
| \FeaturesSymbols that describe features and capabilities of the board
\General Purpose Input/OutputThis is the common API for GPIO