_system_clock_dfll_config | DFLL-specific data container |
 _system_clock_dpll_config | DPLL-specific data container |
 _system_clock_module | System clock module data container |
 _system_clock_xosc_config | XOSC-specific data container |
 EcDomainParam | |
 EcPoint | |
 EFUSEProdStruct | |
 extint_chan_conf | External Interrupt Controller channel configuration structure |
 extint_events | External Interrupt event enable/disable structure |
 extint_nmi_conf | External Interrupt Controller NMI configuration structure |
 in_addr | IPv4 address representation |
 port_config | Port pin configuration structure |
 sha256ctxt | |
 sockaddr | Generic socket address structure |
 sockaddr_in | Socket address structure for IPV4 addresses. Used to specify socket address information to connect to. Can be cast to sockaddr structure |
 spi_config | SPI configuration structure |
 spi_master_config | SPI Master configuration structure |
 spi_module | SERCOM SPI driver software device instance structure |
 spi_slave_config | SPI slave configuration structure |
 spi_slave_inst | SPI peripheral slave instance structure |
 spi_slave_inst_config | SPI peripheral slave configuration structure |
 StructCPtr | Structure of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 StructCVPtr | Structure of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 StructPtr | Structure of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 StructVPtr | Structure of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 system_clock_source_dfll_config | Configuration structure for DFLL |
 system_clock_source_osc32k_config | Configuration structure for OSC32K |
 system_clock_source_osc8m_config | Configuration structure for OSC8M |
 system_clock_source_xosc32k_config | Configuration structure for XOSC32K |
 system_clock_source_xosc_config | Configuration structure for XOSC |
 system_gclk_chan_config | Generic Clock configuration structure |
 system_gclk_gen_config | Generic Clock Generator configuration structure |
 system_pinmux_config | Port pin configuration structure |
 tcc_capture_config | Configuration struct for the TCC module capture |
 tcc_config | TCC configuration structure |
 tcc_counter_config | Configuration struct for the TCC module base counter |
 tcc_events | TCC event enable/disable structure |
 tcc_input_event_config | TCC input event enable/disable/configure structure |
 tcc_match_wave_config | Configuration struct for the TCC module match/wave generation |
 tcc_module | TCC software device instance structure |
 tcc_non_recoverable_fault_config | Configuration struct for TCC module non-recoverable fault |
 tcc_output_event_config | TCC output event enable/disable/configure structure |
 tcc_pins_config | Configuration struct for the TCC module output pins |
 tcc_recoverable_fault_config | Configuration struct for TCC module recoverable fault |
 tcc_wave_extension_config | Configuration struct for the TCC module waveform extension |
 tstr1xAuthCredentials | |
 tstr1xAuthTLSCredentials | |
 tstrAcceptReply | |
 tstrAuth1xMschap2 | |
 tstrAuth1xTls | |
 tstrAuthPsk | |
 tstrAuthWep | |
 tstrBindCmd | |
 tstrBindReply | |
 tstrCloseCmd | |
 tstrConnectAlpnReply | Connect Reply, contains sock number, error value and index of negotiated application protocol |
 tstrConnectCmd | |
 tstrConnectReply | Connect Reply, contains sock number and error value |
 tstrDnsReply | DNS Reply, contains hostName and HostIP |
 tstrEccReqInfo | |
 tstrEcdhReqInfo | |
 tstrECDomainParam | ECC Curve Domain Parameters |
 tstrEcdsaSignReqInfo | |
 tstrEcdsaVerifyReqInfo | |
 tstrECPoint | Elliptic Curve point representation |
 tstrEllipticCurve | Definition of an elliptic curve |
 tstrEthInitParam | Structure to hold Ethernet interface parameters. Structure is to be defined and have its attributes set, based on the application's functionality before a call is made to initialize the wi-fi operations by calling the m2m_wifi_init function. Part of the wi-fi configuration structure tstrWifiInitParam. Applications shouldn't need to define this structure, if the bypass mode is not defined |
 tstrFlashMapEntry | |
 tstrGpRegs | |
 tstrHifContext | |
 tstrHifHdr | Structure to hold HIF header |
 tstrI2cMasterInitParam | I2C master configuration parameters |
 tstrListenCmd | |
 tstrListenReply | |
 tstrM2MAPConfig | This structure holds the configuration parameters for the AP mode. It should be set by the application when it requests to enable the AP operation mode. The AP mode currently supports only OPEN and WEP security |
 tstrM2MAPConfigExt | AP Configuration Extension |
 tstrM2MAPModeConfig | AP Configuration |
 tstrM2mBatteryVoltage | This struct stores the battery voltage |
 tstrM2mBleApiMsg | This struct contains a BLE message |
 tstrM2MBLEInfo | BLE Result |
 tstrM2mClientState | This struct contains the information for the PS Client state |
 tstrM2mConnCredCmn | Wi-Fi Connect Credentials Common section |
 tstrM2mConnCredHdr | Wi-Fi Connect Credentials Header |
 tstrM2MConnInfo | This struct contains the connection information |
 tstrM2MDefaultConnResp | This struct contains the response error of m2m_default_connect |
 tstrM2MDeviceNameConfig | This struct contains the Device Name of the WINC. It is used mainly for Wi-Fi Direct device discovery and WPS device information |
 tstrM2mEnableLogs | This struct stores logging information |
 tstrM2MGainTable | This struct contains the information of the gain table index from flash to be used |
 tstrM2MGainTableRsp | This struct contains response when the firmware has failed to configure the gains from flash |
 tstrM2MGenericResp | Generic success/error response |
 tstrM2MIPConfig | This struct contains the static IP configuration |
 tstrM2mIpCtrlBuf | Structure holding the incoming buffer's data size information, indicating the data size of the buffer and the remaining buffer's data size. The data of the buffer which holds the packet sent to the host when in the bypass mode, is placed in the tstrEthInitParam::au8ethRcvBuf attribute. This following information is retrieved in the host when an event M2M_WIFI_RESP_ETHERNET_RX_PACKET is received in the Wi-Fi callback function tpfAppWifiCb |
 tstrM2mIpRsvdPkt | This struct contains the size and data offset for the received packet |
 tstrM2mLsnInt | This struct contains the Listen Interval. It is the value of the Wi-Fi StA Listen Interval when power save is enabled. It is given in units of Beacon period. It is the number of Beacon periods the WINC can sleep before it wakes up to receive data buffered for it in the AP |
 tstrM2MMulticastMac | This struct contains the information from the Multicast filter |
 tstrM2MP2PConnect | This struct contains the Listen Channel for P2P connect |
 tstrM2MProvisionInfo | This struct contains the provisioning information obtained from the HTTP Provisioning server |
 tstrM2MProvisionModeConfig | This struct contains the provisioning mode configuration |
 tstrM2mPsType | This struct contains the Power Save configuration |
 tstrM2mPwrMode | |
 tstrM2mPwrState | This struct stores the Power Save modes |
 tstrM2mReqScanResult | The Wi-Fi Scan results list is stored in firmware. This struct contains the index by which the application can request a certain scan result |
 tstrM2mRev | Structure holding firmware version parameters and build date/time |
 tstrM2MScan | This struct contains the Wi-Fi scan request |
 tstrM2mScanDone | This struct contains the Wi-Fi scan result |
 tstrM2MScanOption | This struct contains the configuration options for Wi-Fi scan |
 tstrM2MScanRegion | This struct contains the Wi-Fi information for the channel regions |
 tstrM2Mservercmd | This struct contains the information for the PS Server command |
 tstrM2mServerInit | This struct contains the information for the PS Server initialization |
 tstrM2mSetMacAddress | This struct contains the MAC address to be used. The WINC loads the mac address from the efuse by default to the WINC configuration memory, however, the application can overwrite the configuration memory with the mac address indicated from the Host |
 tstrM2mSha256Ctxt | SHA256 context data |
 tstrM2mSlpReqTime | This struct contains the sleep time for the Power Save request |
 tstrM2MSNTPConfig | SNTP Client Configuration |
 tstrM2MStopScanOption | This struct holds additional configuration options for Wi-Fi scan |
 tstrM2mTxPwrLevel | This struct stores the Tx Power levels |
 tstrM2mWifi1xHdr | Wi-Fi Authentication 802.1x header for parameters. The parameters (Domain, UserName, PrivateKey/Password) are appended to this structure |
 tstrM2mWifiApId | Specify an access point (by SSID) |
 tstrM2mWifiAuthInfoHdr | Generic Wi-Fi authentication information to be sent in a separate HIF message of type M2M_WIFI_IND_CONN_PARAM (preceding M2M_WIFI_REQ_CONN) |
 tstrM2mWifiConnectLegacy_1_2 | Wi-Fi Connect Request IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages. For general usage, this structure is replaced by tstrM2mWifiConnHdr |
 tstrM2mWifiConnHdr | Wi-Fi Connect Request (new format) for use with M2M_WIFI_REQ_CONN. This structure is sent across the HIF along with the relevant auth details. One of: tstrM2mWifiPsk tstrM2mWifiWep tstrM2mWifi1xHdr If further authentication details need to be sent (such as client certificate for 1x TLS), they are sent with header tstrM2mWifiAuthInfoHdr in a preceding HIF message of type M2M_WIFI_IND_CONN_PARAM |
 tstrM2MWifiMonitorModeCtrl | This struct contains the Wi-Fi Monitor Mode Filter. It sets the filtering criteria for WLAN packets when monitoring mode is enabled. The received packets matching the filtering parameters, are passed directly to the application |
 tstrM2mWifiPsk | |
 tstrM2mWifiPskInfo | Passphrase and PSK for WPA(2) PSK |
 tstrM2mWiFiRoaming | Roaming related information |
 tstrM2MWifiRxPacketInfo | This struct contains the Wi-Fi RX Frame Header. The M2M application has the ability to allow Wi-Fi monitoring mode for receiving all Wi-Fi Raw frames matching a well defined filtering criteria. When a target Wi-Fi packet is received, the header information are extracted and assigned in this structure |
 tstrM2mWifiscanResult | This struct contains the information corresponding to an AP in the scan result list identified by its order (index) in the list |
 tstrM2MWifiSecInfoLegacy_1_2 | Authentication credentials to connect to a Wi-Fi network. IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages |
 tstrM2mWifiStateChanged | This struct contains the Wi-Fi connection state |
 tstrM2MWifiTxPacketInfo | This struct contains the Wi-Fi TX Packet Info. The M2M Application has the ability to compose raw Wi-Fi frames (under the application responsibility). When transmitting a Wi-Fi packet, the application must supply the firmware with this structure for sending the target frame |
 tstrM2mWifiWep | WEP security key header |
 tstrM2mWifiWepParams | |
 tstrM2mWifiWepParamsLegacy_1_2 | WEP security key parameters. IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages |
 tstrM2MWPSConnect | This struct stores the WPS configuration parameters |
 tstrM2MWPSInfo | WPS Result |
 tstrNetworkId | |
 tstrNmBusCapabilities | Structure holding bus capabilities information |
 tstrNmI2cDefault | Structure holding I2C default operation parameters |
 tstrNmI2cSpecial | Structure holding I2C special operation parameters |
 tstrNmSpiRw | Structure holding SPI R/W parameters |
 tstrNmUartDefault | Structure holding UART default operation parameters |
 tstrOtaControlSec | Control Section Structure. The Control Section is used to define the working image and the validity of the roll-back image and its offset, also both firmware versions are kept in this structure |
 tstrOtaInitHdr | This struct contains the OTA image header |
 tstrOtaUpdateInfo | This struct contains the OTA update information |
 tstrOtaUpdateStatusResp | This struct contains the OTA update status |
 tstrPerphInitParam | Peripheral module initialization parameters |
 tstrPingCmd | |
 tstrPingReply | |
 tstrPrng | M2M Request PRNG |
 tstrRecvCmd | |
 tstrRecvReply | |
 tstrRootCertEcdsaKeyInfo | Info about a ECDSA public key |
 tstrRootCertEntryHeader | Header of a root certificate entry in flash |
 tstrRootCertFlashHeader | Header of the root certificate flash storage area |
 tstrRootCertPubKeyInfo | Info about the public key contained in a root certificate |
 tstrRootCertRsaKeyInfo | Info about a RSA public key |
 tstrSendCmd | |
 tstrSendReply | Send Reply, contains socket number and number of sent bytes |
 tstrSetSocketOptCmd | |
 tstrSockAddr | |
 tstrSockErr | Detail about socket failures. Used with get_error_detail |
 tstrSocket | |
 tstrSocketAcceptMsg | Socket accept status |
 tstrSocketBindMsg | Socket bind status |
 tstrSocketConnectMsg | Socket connect status |
 tstrSocketListenMsg | Socket listen status |
 tstrSocketRecvMsg | Socket recv status |
 tstrSslSetActiveCsList | |
 tstrSSLSetSockOptCmd | |
 tstrSSLSocketCreateCmd | |
 tstrSystemTime | This struct contains the system time |
 tstrTimer | |
 tstrTlsSrvChunkHdr | |
 tstrTlsSrvSecFileEntry | This struct contains a TLS certificate |
 tstrTlsSrvSecHdr | This struct contains a set of TLS certificates |
 tstrWakeTimer | |
 tstrWifiInitParam | Structure, holding the Wi-fi configuration attributes such as the wi-fi callback , monitoring mode callback and Ethernet parameter initialization structure. |
 tuniM2MWifiAuthLegacy_1_2 | Wi-Fi Security Parameters for all supported security modes. IMPORTANT: This structure is required only for legacy M2M_WIFI_REQ_CONNECT messages |
 Union16 | 16-bit union |
 Union32 | 32-bit union |
 Union64 | 64-bit union |
 UnionCPtr | Union of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 UnionCVPtr | Union of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 UnionPtr | Union of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 UnionVPtr | Union of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 usart_config | USART configuration struct |
 usart_module | SERCOM USART driver software device instance structure |
 wifiProvisionParams | |