This example demonstrates the use of the WINC3400 with the SAMD21 Xplained Pro board to start Wi-Fi provisioning mode using simple HTTPS server implemented in SAMD21. This example support provisioning in following Wi-Fi Security mode.
It uses the following hardware:
This software was written for the GNU GCC compiler using Atmel Studio 7 Other compilers are not guaranteed to work. Provisioning web page has been tested in Google chrome and Firefox. The web page may not work perfectly in other browser.
For further information, visit Microchip.