Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
WINC3400 Send Email Example - SAMD21 XPlained Pro Documentation

Introduction

This example demonstrates the use of the WINC3400 with the SAMD21 Xplained Pro board to send email using SMTP server.
It uses the following hardware:

  • the SAMD21 Xplained Pro.
  • the WINC3400 on EXT1.

Main Files

  • main.c : Initialize the WINC3400 and send email.

Usage

  1. Configure below code in the main.h for AP information to be connected.
    * #define MAIN_WLAN_SSID "DEMO_AP"
    * #define MAIN_WLAN_PSK "12345678"
    *
    * #define MAIN_SENDER_RFC "<sender@gmail.com>"
    * #define MAIN_RECIPIENT_RFC "<recipient@gmail.com>"
    * #define MAIN_TO_ADDRESS "recipient@gmail.com"
    * #define MAIN_FROM_ADDRESS "sender@gmail.com"
    * #define MAIN_FROM_PASSWORD "12345678"
    *
  2. Build the program and download it into the board.
  3. On the computer, open and configure a terminal application as the follows.
    * Baud Rate : 115200
    * Data : 8bit
    * Parity bit : none
    * Stop bit : 1bit
    * Flow control : none
    *
  4. Start the application.
  5. In the terminal window, the following text should appear:
    * -- WINC3400 send email example --
    * -- Compiled: xxx xx xxxx xx:xx:xx --
    * wifi_cb: M2M_WIFI_REQ_DHCP_CONF: IP is xxx.xxx.xxx.xxx
    * Host IP is 173.194.72.108
    * Host Name is smtp.gmail.com
    * Recipient email address is recipient@gmail.com
    * main: Email was successfully sent.
    *
Warning
* For using the GMAIL, the root certificate must be installed.
* Download the root certificate using the root_certificate_downloader. (Refer to WINC3400 Software User Guide.)
*

Compilation Information

This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers are not guaranteed to work.

Contact Information

For further information, visit Microchip.