Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
WINC3400 Serial Bridge Example - SAM4S XPlained Pro Documentation

Introduction

This example demonstrates how to implement a EDBG UART to WINC3400 SPI bridge.
It uses the following hardware:

  • the SAM Xplained Pro.
  • the WINC3400 on EXT1.

Main Files

Usage

  1. Build the program and download it into the board.
  2. Run download_all.bat script in firmware_update_project

Compilation Information

This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers are not guaranteed to work.

Contact Information

For further information, visit Microchip.