Introduction
This example demonstrates how to implement a EDBG UART to WINC3400 SPI bridge.
It uses the following hardware:
- the SAM Xplained Pro.
- the WINC3400 on EXT1.
Main Files
- serial_bridge.c : Initialize the WINC3400 perform bridge operation.
Usage
- Build the program and download it into the board.
- Run download_all.bat script in firmware_update_project
Compilation Information
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers are not guaranteed to work.
Contact Information
For further information, visit Microchip.