Microchip® Advanced Software Framework

tstrM2mIpCtrlBuf Struct Reference

Structure holding the incoming buffer's data size information, indicating the data size of the buffer and the remaining buffer's data size. The data of the buffer which holds the packet sent to the host when in the bypass mode, is placed in the tstrEthInitParam::au8ethRcvBuf attribute. This following information is retrieved in the host when an event M2M_WIFI_RESP_ETHERNET_RX_PACKET is received in the Wi-Fi callback function tpfAppWifiCb.

The application is expected to use this structure's information to determine if there is still incoming data to be received from the firmware.
See Also
tpfAppWifiCb tpfAppEthCb tstrEthInitParam
Warning
Make sure that ETHERNET/bypass mode is defined before using tstrM2mIpCtrlBuf

#include <m2m_wifi.h>

Data Fields

uint16 u16DataSize
 
uint16 u16RemainingDataSize
 

uint16 tstrM2mIpCtrlBuf::u16DataSize

Size of the received data in bytes.

Referenced by m2m_wifi_cb().

uint16 tstrM2mIpCtrlBuf::u16RemainingDataSize

Size of the remaining data bytes to be delivered to host.

Referenced by m2m_wifi_cb().