Microchip® Advanced Software Framework

tstrM2mSetMacAddress Struct Reference

This struct contains the MAC address to be used. The WINC loads the mac address from the efuse by default to the WINC configuration memory, however, the application can overwrite the configuration memory with the mac address indicated from the Host.

Note
It's recommended to call this only once before calling connect request and after the m2m_wifi_init

#include <m2m_types.h>

Data Fields

uint8 __PAD16__ [2]
 
uint8 au8Mac [6]
 

uint8 tstrM2mSetMacAddress::__PAD16__[2]

Padding bytes for forcing 4-byte alignment

uint8 tstrM2mSetMacAddress::au8Mac[6]

MAC address

Referenced by m2m_wifi_set_mac_address().