Introduction
This example demonstrates the use of the WINC3400 with the SAM Xplained Pro board to check the signal strength such as RSSI.
It uses the following hardware:
- the SAM Xplained Pro.
- the WINC3400 on EXT1.
Main Files
- main.c : Initialize the WINC3400 and get RSSI for the connected AP.
Usage
- Configure below code in the config main.h for AP to connect to.
- Build the program and download it into the board.
- On the computer, open and configure a terminal application as the follows.
* Baud Rate : 115200
* Data : 8bit
* Parity bit : none
* Stop bit : 1bit
* Flow control : none
*
- Start the application.
- In the terminal window, the following text should appear:
* -- WINC3400 signal statistics example --
* -- Compiled: xxx xx xxxx xx:xx:xx --
* Wi-Fi connected
* Wi-Fi IP is xxx.xxx.xxx.xxx
* RSSI for the current connected AP (-48)
*
Compilation Information
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers are not guaranteed to work.
Contact Information
For further information, visit Microchip.