Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Roaming

        Here are listed all the functions that implement the Wifi Roaming APIs.

Functions

sint8 m2m_wifi_disable_roaming (void)
 Disable WiFi STA roaming. More...
 
sint8 m2m_wifi_enable_roaming (uint8 bEnableDhcp)
 Enable WiFi STA roaming. More...
 

sint8 m2m_wifi_disable_roaming ( void  )

Disable WiFi STA roaming.

Precondition
Must be called after the initialization.
Returns
The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
See Also
m2m_wifi_init

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_ROAMING, NULL, and tstrM2mWiFiRoaming::u8EnableRoaming.

sint8 m2m_wifi_enable_roaming ( uint8  bEnableDhcp)

Enable WiFi STA roaming.

m2m_wifi_enable_roaming enables the firmware to trigger the roaming algorithm/steps on link loss with the current AP.
If roaming is successful, the @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_ROAMED is sent to the host.
Additionally a @ref M2M_WIFI_REQ_DHCP_CONF message with new DHCP lease details is sent to host (only if bEnableDhcp=1).
If roaming is unsuccessful, a @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_DISCONNECTED is sent to host.
Parameters
[in]bEnableDhcp0 : Disables DHCP client execution after roaming to new AP 1 : Enables DHCP client execution after roaming to new AP
Precondition
Must be called after the initialization. The roaming algorithm/procedure is internal to the firmware.
Returns
The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
See Also
m2m_wifi_init

References hif_send(), M2M_ERR_INVALID_ARG, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_ROAMING, NULL, tstrM2mWiFiRoaming::u8EnableDhcp, and tstrM2mWiFiRoaming::u8EnableRoaming.

Referenced by main().