Microchip® Advanced Software Framework

tstrM2mReqScanResult Struct Reference

The Wi-Fi Scan results list is stored in firmware. This struct contains the index by which the application can request a certain scan result.

#include <m2m_types.h>

Data Fields

uint8 __PAD24__ [3]
 
uint8 u8Index
 

uint8 tstrM2mReqScanResult::__PAD24__[3]

Padding bytes for forcing 4-byte alignment

uint8 tstrM2mReqScanResult::u8Index

Index of the desired scan result

Referenced by m2m_wifi_req_scan_result().