Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Bypass Mode

        Here are listed all the functions that implement the Bypass Mode APIs.

Functions

sint8 m2m_wifi_send_ethernet_pkt (uint8 *pu8Packet, uint16 u16PacketSize)
 Asynchronous API to queue an Ethernet packet for transmission by the WINC. More...
 

NMI_API sint8 m2m_wifi_send_ethernet_pkt ( uint8 pu8Packet,
uint16  u16PacketSize 
)

Asynchronous API to queue an Ethernet packet for transmission by the WINC.

Transmit a packet directly in ETHERNET/bypass mode where the TCP/IP stack is disabled
and the implementation of this packet is left to the application developer.
The Ethernet packet composition is left to the application developer.
Note
Packets are the user's responsibility.
Warning
This function available in ETHERNET/Bypass mode ONLY. Make sure that application defines ETH_MODE.
Parameters
[in]pu8PacketPointer to a buffer holding the whole Ethernet frame.
[in]u16PacketSizeThe size of the whole packet in bytes.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
m2m_wifi_enable_mac_mcast m2m_wifi_set_receive_buffer

References hif_send(), M2M_ETHERNET_HDR_LEN, M2M_ETHERNET_HDR_OFFSET, M2M_HIF_HDR_OFFSET, M2M_REQ_DATA_PKT, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_SEND_ETHERNET_PACKET, NULL, tstrM2MWifiTxPacketInfo::u16HeaderLength, and tstrM2MWifiTxPacketInfo::u16PacketSize.