Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Hot-Spot (Access-Point)

        Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs.

Functions

sint8 m2m_wifi_disable_ap (void)
 Synchronous API to disable access point mode on the WINC. More...
 
sint8 m2m_wifi_enable_ap (CONST tstrM2MAPConfig *pstrM2MAPConfig)
 Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC. More...
 
sint8 m2m_wifi_enable_ap_ext (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig)
 Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC with extended options. More...
 

NMI_API sint8 m2m_wifi_disable_ap ( void  )

Synchronous API to disable access point mode on the WINC.

Must be called only when the AP is enabled through the @ref m2m_wifi_enable_ap
function. Otherwise the call to this function will not be useful.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
m2m_wifi_enable_ap

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_DISABLE_AP, and NULL.

NMI_API sint8 m2m_wifi_enable_ap ( CONST tstrM2MAPConfig pstrM2MAPConfig)

Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC.

The WINC supports the ability to operate as an access point with the following limitations:
- Only 1 station may be associated at any given time.
- Open system and WEP are the only security suites supported.
Parameters
[in]pstrM2MAPConfigA structure holding the AP configurations.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
Warning
This function is not allowed in P2P or STA modes.
Precondition
See Also
tpfAppWifiCb tenuM2mSecType m2m_wifi_init M2M_WIFI_REQ_DHCP_CONF tstrM2mWifiStateChanged tstrM2MAPConfig

Example

The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.

#include "m2m_wifi.h"
#include "m2m_types.h"
void wifi_event_cb(uint8 u8WiFiEvent, void * pvMsg)
{
switch(u8WiFiEvent)
{
{
uint8 *pu8IPAddress = (uint8*)pvMsg;
printf("Associated STA has IP Address \"%u.%u.%u.%u\"\n",pu8IPAddress[0],pu8IPAddress[1],pu8IPAddress[2],pu8IPAddress[3]);
}
break;
default:
break;
}
}
int main()
{
param.pfAppWifiCb = wifi_event_cb;
if(!m2m_wifi_init(&param))
{
tstrM2MAPConfig apConfig;
strcpy(apConfig.au8SSID, "WINC_SSID");
apConfig.u8ListenChannel = 1;
apConfig.u8SsidHide = 0;
// IP Address
apConfig.au8DHCPServerIP[0] = 192;
apConfig.au8DHCPServerIP[1] = 168;
apConfig.au8DHCPServerIP[2] = 1;
apConfig.au8DHCPServerIP[3] = 1;
// Trigger AP
m2m_wifi_enable_ap(&apConfig);
while(1)
{
}
}
}

References tstrM2MAPConfigExt::au8DefRouterIP, tstrM2MAPConfigExt::au8DNSServerIP, tstrM2MAPConfigExt::au8SubnetMask, m2m_memcpy(), m2m_wifi_enable_ap_ext(), tstrM2MAPModeConfig::strApConfig, and tstrM2MAPModeConfig::strApConfigExt.

NMI_API sint8 m2m_wifi_enable_ap_ext ( CONST tstrM2MAPModeConfig pstrM2MAPModeConfig)

Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC with extended options.

The WINC supports the ability to operate as an access point with the following limitations:
- Only 1 station may be associated at any given time.
- Open system and WEP are the only security suites supported.
Parameters
[in]pstrM2MAPModeConfigA structure holding the AP configurations.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
Warning
This function is not allowed in P2P or STA modes.
Precondition
See Also
tpfAppWifiCb tenuM2mSecType m2m_wifi_init M2M_WIFI_REQ_DHCP_CONF tstrM2mWifiStateChanged tstrM2MAPModeConfig

Example

The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.

#include "m2m_wifi.h"
#include "m2m_types.h"
void wifi_event_cb(uint8 u8WiFiEvent, void * pvMsg)
{
switch(u8WiFiEvent)
{
{
uint8 *pu8IPAddress = (uint8*)pvMsg;
printf("Associated STA has IP Address \"%u.%u.%u.%u\"\n",pu8IPAddress[0],pu8IPAddress[1],pu8IPAddress[2],pu8IPAddress[3]);
}
break;
default:
break;
}
}
int main()
{
param.pfAppWifiCb = wifi_event_cb;
if(!m2m_wifi_init(&param))
{
tstrM2MAPModeConfig apModeConfig;
strcpy(apModeConfig.strApConfig.au8SSID, "WINC_SSID");
apModeConfig.strApConfig.u8ListenChannel = 1;
apModeConfig.strApConfig.u8SsidHide = 0;
// IP Address
apModeConfig.strApConfig.au8DHCPServerIP[0] = 192;
apModeConfig.strApConfig.au8DHCPServerIP[1] = 168;
apModeConfig.strApConfig.au8DHCPServerIP[2] = 1;
apModeConfig.strApConfig.au8DHCPServerIP[3] = 1;
// Default router IP
// DNS Server IP
// Subnet mask
apModeConfig.strApConfigExt.au8SubnetMask[0] = 255;
apModeConfig.strApConfigExt.au8SubnetMask[1] = 255;
apModeConfig.strApConfigExt.au8SubnetMask[2] = 255;
apModeConfig.strApConfigExt.au8SubnetMask[3] = 0;
// Trigger AP
m2m_wifi_enable_ap_ext(&apModeConfig);
while(1)
{
}
}
}

References hif_send(), M2M_ERR_FAIL, M2M_ERR_SEND, M2M_REQ_GROUP_WIFI, M2M_SUCCESS, m2m_validate_ap_parameters(), M2M_WIFI_REQ_ENABLE_AP, M2M_WIFI_REQ_ENABLE_AP_LEGACY, and NULL.

Referenced by m2m_wifi_enable_ap().