Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
WINC3400 (Wi-Fi + BLE)

Macros

#define WIFI_1X_TLS_HS_FLAGS_DEFAULT
 
#define WIFI_1X_TLS_HS_FLAGS_PEER_AUTH   NBIT1
 
#define WIFI_1X_TLS_HS_FLAGS_PEER_CERTTIMECHECK   NBIT2
 
#define WIFI_1X_TLS_HS_FLAGS_REQUIRE_TIME   NBIT3
 
#define WIFI_1X_TLS_HS_FLAGS_SESSION_CACHING   NBIT4
 
#define WIFI_1X_TLS_HS_FLAGS_SPECIFY_ROOTCERT   NBIT6
 

Functions

static sint8 legacy_connect_prepare_msg (tstrM2mWifiConnHdr *pstrConnHdr, tstrM2mWifiConnectLegacy_1_2 *pstrConnect)
 
static sint8 m2m_validate_ap_parameters (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig)
 
static sint8 m2m_validate_scan_options (tstrM2MScanOption *ptstrM2MScanOption)
 
static void m2m_wifi_cb (uint8 u8OpCode, uint16 u16DataSize, uint32 u32Addr)
 
static sint8 m2m_wifi_connect_prepare_msg (tenuCredStoreOption enuCredStoreOption, tenuM2mSecType enuAuthType, uint16 u16AuthSize, tstrNetworkId *pstrNetworkId, tstrM2mWifiConnHdr *pstrWifiConn)
 
sint8 m2m_wifi_enable_firmware_logs (uint8 u8Enable)
 Enable or Disable logs in run time (Disable Firmware logs will enhance the firmware start-up time and performance) More...
 
uint32 m2m_wifi_get_chipId (void)
 Get the WINC Chip ID. More...
 
sint8 m2m_wifi_p2p (uint8 u8Channel)
 
sint8 m2m_wifi_p2p_disconnect (void)
 
sint8 m2m_wifi_wps (uint8 u8TriggerType, const char *pcPinNumber)
 Asynchronous API to engage the WINC Wi-Fi Protected Setup (enrollee) function. More...
 
sint8 m2m_wifi_wps_disable (void)
 Asynchronous API that disables Wi-Fi Protected Setup mode in the WINC. More...
 

Variables

static uint8 gau81xRootSha1 [20] = {0}
 
static tpfAppWifiCb gpfAppWifiCb = NULL
 
static uint32 gu321xTlsHsFlags = WIFI_1X_TLS_HS_FLAGS_DEFAULT
 
static volatile uint8 gu8ChNum
 

#define WIFI_1X_TLS_HS_FLAGS_DEFAULT
Value:
( \
)
#define WIFI_1X_TLS_HS_FLAGS_SESSION_CACHING
Definition: m2m_wifi.c:49
#define WIFI_1X_TLS_HS_FLAGS_PEER_AUTH
Definition: m2m_wifi.c:46
#define WIFI_1X_TLS_HS_FLAGS_PEER_CERTTIMECHECK
Definition: m2m_wifi.c:47
#define WIFI_1X_TLS_HS_FLAGS_PEER_AUTH   NBIT1
#define WIFI_1X_TLS_HS_FLAGS_PEER_CERTTIMECHECK   NBIT2
#define WIFI_1X_TLS_HS_FLAGS_REQUIRE_TIME   NBIT3
#define WIFI_1X_TLS_HS_FLAGS_SESSION_CACHING   NBIT4
#define WIFI_1X_TLS_HS_FLAGS_SPECIFY_ROOTCERT   NBIT6

NMI_API sint8 m2m_wifi_enable_firmware_logs ( uint8  u8Enable)

Enable or Disable logs in run time (Disable Firmware logs will enhance the firmware start-up time and performance)

Enable or Disable logs in run time.

Parameters
[in]u8EnableSet 1 to enable the logs 0 for disable
Returns
The function SHALL return M2M_SUCCESS for success and a negative value otherwise.
See Also
DISABLE_FIRMWARE_LOGS (build option to disable logs from initializations)
Precondition
m2m_wifi_init
Warning
Enable or Disable logs in run time (Disable Firmware logs will enhance the firmware start-up time and performance).
Parameters
[in]u8EnableSet 1 to enable the logs, 0 for disable.
Precondition
Must be called after initialization through the following function m2m_wifi_init.
Returns
The function returns M2M_SUCCESS for success and a negative value otherwise.
See Also
DISABLE_FIRMWARE_LOGS (build option to disable logs from initializations) m2m_wifi_init

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_SET_ENABLE_LOGS, NULL, and tstrM2mEnableLogs::u8Enable.

uint32 m2m_wifi_get_chipId ( void  )

Get the WINC Chip ID.

Synchronous API to obtain the firmware WINC chip ID.

Returns
The function SHALL return chipID >0 or 0 for failure.
The function returns chipID > 0 or 0 for failure.

References nmi_get_chipid().

sint8 m2m_wifi_p2p_disconnect ( void  )
NMI_API sint8 m2m_wifi_wps ( uint8  u8TriggerType,
const char *  pcPinNumber 
)

Asynchronous API to engage the WINC Wi-Fi Protected Setup (enrollee) function.

This function can be called to make the WINC enter WPS (Wi-Fi Protected Setup) mode. The result
is passed to the Wi-Fi notification callback with the event @ref M2M_WIFI_REQ_WPS.
Parameters
[in]u8TriggerTypeWPS Trigger method. This may be:
[in]pcPinNumberValid only if the u8TriggerType is WPS_PIN_TRIGGER, this parameter contains the PIN number. The number must follow the format as given in the WSC1.0 specification.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
Warning
This function is not allowed in AP or P2P modes.
Precondition
  • A Wi-Fi notification callback of type (tpfAppWifiCb MUST be implemented and registered at startup. Registering the callback is done through passing it to m2m_wifi_init.
  • The event M2M_WIFI_REQ_WPS must be handled in the callback to receive the WPS status.
  • The WINC device MUST be in IDLE or STA mode. If AP or P2P mode is active, the WPS will not be performed.
  • The m2m_wifi_handle_events MUST be called periodically to receive the responses in the callback.
See Also
tpfAppWifiCb m2m_wifi_init M2M_WIFI_REQ_WPS tenuWPSTrigger tstrM2MWPSInfo

Example

The code snippet shows an example of how wi-fi WPS is triggered .

#include "m2m_wifi.h"
#include "m2m_types.h"
void wifi_event_cb(uint8 u8WiFiEvent, void * pvMsg)
{
switch(u8WiFiEvent)
{
{
tstrM2MWPSInfo *pstrWPS = (tstrM2MWPSInfo*)pvMsg;
if(pstrWPS->u8AuthType != 0)
{
// establish Wi-Fi connection
tstrNetworkId strNetworkId = {NULL, pstrWPS->au8SSID, (uint8)strlen((char*)(pstrWPS->au8SSID)), pstrWPS->u8Ch};
if(pstrWPS->u8AuthType == M2M_WIFI_SEC_OPEN)
{
}
else
{
tstrAuthPsk strAuthPsk = {NULL, pstrWPS->au8PSK, (uint8)strlen((char*)(pstrWPS->au8PSK))};
m2m_wifi_connect_psk(WIFI_CRED_SAVE_ENCRYPTED, &strNetworkId, &strAuthPsk);
}
printf("WPS SSID : %s\n",pstrWPS->au8SSID);
printf("WPS PSK : %s\n",pstrWPS->au8PSK);
printf("WPS SSID Auth Type : %s\n",pstrWPS->u8AuthType == M2M_WIFI_SEC_OPEN ? "OPEN" : "WPA/WPA2");
printf("WPS Channel : %d\n",pstrWPS->u8Ch);
}
else
{
printf("(ERR) WPS Is not enabled OR Timed out\n");
}
}
break;
default:
break;
}
}
int main()
{
param.pfAppWifiCb = wifi_event_cb;
if(!m2m_wifi_init(&param))
{
// Trigger WPS in Push button mode.
while(1)
{
}
}
}

References tstrM2MWPSConnect::acPinNumber, hif_send(), m2m_memcpy(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_WPS, NULL, tstrM2MWPSConnect::u8TriggerType, and WPS_PIN_TRIGGER.

NMI_API sint8 m2m_wifi_wps_disable ( void  )

Asynchronous API that disables Wi-Fi Protected Setup mode in the WINC.

Precondition
WINC should be already in WPS mode using m2m_wifi_wps.
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
m2m_wifi_wps

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_DISABLE_WPS, and NULL.

tpfAppWifiCb gpfAppWifiCb = NULL
static

Referenced by m2m_wifi_cb(), and m2m_wifi_init_start().

volatile uint8 gu8ChNum
static