Microchip® Advanced Software Framework

sockaddr Struct Reference

Generic socket address structure.

See Also
sockaddr_in

#include <socket.h>

Data Fields

uint8 sa_data [14]
 
uint16 sa_family
 

uint8 sockaddr::sa_data[14]

Maximum size of all the different socket address structures.

uint16 sockaddr::sa_family

Socket address family.