Here are listed all the functions that implement the Wifi Crypto APIs.
Functions | |
sint8 | m2m_wifi_prng_get_random_bytes (uint8 *pu8PrngBuff, uint16 u16PrngSize) |
Get random bytes using the PRNG bytes. More... | |
Get random bytes using the PRNG bytes.
Asynchronous function for retrieving from the firmware a pseudo-random set of bytes.
[in] | u16PrngSize | Size of the required random bytes to be generated. |
[in] | pu8PrngBuff | Pointer to user allocated buffer. |
Asynchronous function for retrieving from the firmware a pseudo-random set of bytes as specified in the size passed in as a parameter. The registered wifi-cb function retrieves the random bytes through the response @ref M2M_WIFI_RESP_GET_PRNG
[in] | pu8PrngBuff | Pointer to a buffer to receive data. |
[in] | u16PrngSize | Request size in bytes |
References hif_send(), M2M_BUFFER_MAX_SIZE, M2M_ERR, M2M_ERR_FAIL, M2M_REQ_DATA_PKT, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_GET_PRNG, NULL, tstrPrng::pu8RngBuff, and tstrPrng::u16PrngSize.