Connect Reply, contains sock number and error value.
#include <m2m_socket_host_if.h>
Data Fields | |
union { | |
struct { | |
uint8 u8ErrCode | |
uint8 u8ErrSource | |
} | |
uint16 u16AppDataOffset | |
}; | |
sint8 | s8Error |
SOCKET | sock |
union { ... } |
sint8 tstrConnectReply::s8Error |
0 for successful connection, in which case u16AppDataOffset is valid. Negative for failed connection, in which case u8ErrorType and u8ErrorDetail may give more info.
Referenced by m2m_ip_cb().
SOCKET tstrConnectReply::sock |
Referenced by m2m_ip_cb().
uint16 tstrConnectReply::u16AppDataOffset |
In further packet send requests the host interface should put the user application data at this offset in the allocated shared data packet.
Referenced by m2m_ip_cb().
uint8 tstrConnectReply::u8ErrCode |
For TLS Alerts, this is the Alert ID.
Referenced by m2m_ip_cb().
uint8 tstrConnectReply::u8ErrSource |
0: No detail 1: TLS Alert received from peer 2: TLS Alert generated locally
Referenced by m2m_ip_cb().