Microchip® Advanced Software Framework

tstrM2MScanRegion Struct Reference

This struct contains the Wi-Fi information for the channel regions.

See Also
tenuM2mScanRegion

#include <m2m_types.h>

Data Fields

uint8 __PAD16__ [2]
 
uint16 u16ScanRegion
 

uint8 tstrM2MScanRegion::__PAD16__[2]

Padding bytes for forcing 4-byte alignment

uint16 tstrM2MScanRegion::u16ScanRegion