This struct contains the OTA update information.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD8__ |
uint8 | u8DownloadUrlOffset |
uint8 | u8DownloadUrlSize |
uint8 | u8NcdRequiredUpgrade |
uint32 | u8NcdUpgradeVersion |
uint32 | u8NcfCurrentVersion |
uint32 | u8NcfUpgradeVersion |
uint8 tstrOtaUpdateInfo::__PAD8__ |
Padding bytes for forcing 4-byte alignment
uint8 tstrOtaUpdateInfo::u8DownloadUrlOffset |
Download URL offset in the received packet
uint8 tstrOtaUpdateInfo::u8DownloadUrlSize |
Download URL size in the received packet
uint8 tstrOtaUpdateInfo::u8NcdRequiredUpgrade |
NCD Required upgrade to the above version
uint32 tstrOtaUpdateInfo::u8NcdUpgradeVersion |
NCD (host) upgraded version (if the u8NcdRequiredUpgrade == true)
uint32 tstrOtaUpdateInfo::u8NcfCurrentVersion |
NCF OTA Current firmware version
uint32 tstrOtaUpdateInfo::u8NcfUpgradeVersion |
NCF OTA Upgrade Version