AT86RFx driver.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
#include "board.h"
#include "conf_at86rfx.h"
#include "spi_master.h"
#include "gpio.h"
#include "at86rfx_driver.h"
Macros | |
#define | CURRENT_CHANNEL_DEFAULT (1) |
Functions | |
at86rfx_retval_t | at86rfx_init (void) |
Initializes the transceiver interface. More... | |
void | at86rfx_task (void) |
RF task handling. More... | |
void | at86rfx_tx_frame (uint8_t *frame_tx) |
Transmits the frame. More... | |
ISR (ext_int_isr, EXT_INT_ISR_GROUP, EXT_INT_ISR_PRIORITY) | |
ISR for transceiver's main interrupt. More... | |
uint8_t | pal_trx_bit_read (uint8_t addr, uint8_t mask, uint8_t pos) |
Subregister read. More... | |
void | pal_trx_bit_write (uint8_t reg_addr, uint8_t mask, uint8_t pos, uint8_t new_value) |
Subregister write. More... | |
void | pal_trx_frame_read (uint8_t *data, uint8_t length) |
Reads frame buffer of the transceiver. More... | |
void | pal_trx_frame_write (uint8_t *data, uint8_t length) |
Writes data into frame buffer of the transceiver. More... | |
void | pal_trx_init (void) |
Initializes the SPI and GPIO pins for transceiver access. More... | |
uint8_t | pal_trx_reg_read (uint8_t addr) |
Reads current value from a transceiver register. More... | |
void | pal_trx_reg_write (uint8_t addr, uint8_t data) |
Writes data into a transceiver register. More... | |
Variables | |
bool | at86rfx_frame_rx = false |
uint8_t | at86rfx_rx_buffer [LARGE_BUFFER_SIZE] |
Static receive buffer that can be used to upload a frame from the trx. More... | |
struct spi_device | SPI_AT86RFX_DEVICE |
#define CURRENT_CHANNEL_DEFAULT (1) |
Referenced by at86rfx_init().
ISR | ( | ext_int_isr | , |
EXT_INT_ISR_GROUP | , | ||
EXT_INT_ISR_PRIORITY | |||
) |
ISR for transceiver's main interrupt.
References CLEAR_TRX_IRQ, and trx_irq_handler_cb().
Referenced by at86rfx_task(), and handle_received_frame_irq().
struct spi_device SPI_AT86RFX_DEVICE |