Microchip® Advanced Software Framework

conf_nvm_example.h File Reference

NVM example configuration.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "uc3/flash_api.h"

Macros

#define NVM_EXAMPLE_LED0   LED0_GPIO
 
#define NVM_EXAMPLE_LED1   LED1_GPIO
 
#define NVM_EXAMPLE_LED2   LED2_GPIO
 
#define TEST_ADDRESS_EXT   (2 * AT45DBX_SECTOR_SIZE)
 
#define TEST_ADDRESS_INT   (FLASH_API_BASE_ADDRESS + FLASH_API_SIZE - FLASH_API_PAGE_SIZE)
 

#define NVM_EXAMPLE_LED0   LED0_GPIO

Referenced by main().

#define NVM_EXAMPLE_LED1   LED1_GPIO

Referenced by main().

#define NVM_EXAMPLE_LED2   LED2_GPIO

Referenced by main().

#define TEST_ADDRESS_EXT   (2 * AT45DBX_SECTOR_SIZE)

Referenced by main().

#define TEST_ADDRESS_INT   (FLASH_API_BASE_ADDRESS + FLASH_API_SIZE - FLASH_API_PAGE_SIZE)

Referenced by main().