Generic clocks are configurable clocks which run outside the system clock domain.
They are often connected to peripherals which have an asynchronous component running independently of the bus clock, e.g. USB controllers, low-power timers and RTCs, etc.
Note that not all platforms have support for generic clocks; on such platforms, this API will not be available.
Data Structures | |
struct | genclk_config |
Hardware representation of a set of generic clock parameters. More... | |
Enumerations | |
enum | genclk_source { GENCLK_PCK_SRC_SLCK_RC = 0, GENCLK_PCK_SRC_SLCK_XTAL = 1, GENCLK_PCK_SRC_SLCK_BYPASS = 2, GENCLK_PCK_SRC_MAINCK_4M_RC = 3, GENCLK_PCK_SRC_MAINCK_8M_RC = 4, GENCLK_PCK_SRC_MAINCK_12M_RC = 5, GENCLK_PCK_SRC_MAINCK_XTAL = 6, GENCLK_PCK_SRC_MAINCK_BYPASS = 7, GENCLK_PCK_SRC_PLLACK = 8, GENCLK_PCK_SRC_PLLBCK = 9, GENCLK_PCK_SRC_MCK = 10 } |
Generic clock source ID. More... | |
Functions | |
static void | genclk_config_defaults (struct genclk_config *p_cfg, uint32_t ul_id) |
static void | genclk_config_read (struct genclk_config *p_cfg, uint32_t ul_id) |
static void | genclk_config_write (const struct genclk_config *p_cfg, uint32_t ul_id) |
static void | genclk_disable (uint32_t ul_id) |
static void | genclk_enable (const struct genclk_config *p_cfg, uint32_t ul_id) |
static void | genclk_enable_config (unsigned int id, enum genclk_source src, unsigned int divider) |
Enable the configuration defined by src and divider for the generic clock identified by id. More... | |
Generic clock configuration | |
static void | genclk_enable_source (enum genclk_source e_src) |
Enable the source clock src used by a generic clock. More... | |
Programmable Clock Identifiers (PCK) | |
#define | GENCLK_PCK_0 0 |
PCK0 ID. More... | |
#define | GENCLK_PCK_1 1 |
PCK1 ID. More... | |
#define | GENCLK_PCK_2 2 |
PCK2 ID. More... | |
Programmable Clock Prescalers (PCK) | |
enum | genclk_divider { GENCLK_PCK_PRES_1 = PMC_PCK_PRES_CLK_1, GENCLK_PCK_PRES_2 = PMC_PCK_PRES_CLK_2, GENCLK_PCK_PRES_4 = PMC_PCK_PRES_CLK_4, GENCLK_PCK_PRES_8 = PMC_PCK_PRES_CLK_8, GENCLK_PCK_PRES_16 = PMC_PCK_PRES_CLK_16, GENCLK_PCK_PRES_32 = PMC_PCK_PRES_CLK_32, GENCLK_PCK_PRES_64 = PMC_PCK_PRES_CLK_64 } |
Programmable Clock Source and Prescaler configuration | |
static void | genclk_config_set_source (struct genclk_config *p_cfg, enum genclk_source e_src) |
Select a new source clock src in configuration cfg. More... | |
static void | genclk_config_set_divider (struct genclk_config *p_cfg, uint32_t e_divider) |
#define GENCLK_PCK_0 0 |
PCK0 ID.
#define GENCLK_PCK_1 1 |
PCK1 ID.
#define GENCLK_PCK_2 2 |
PCK2 ID.
enum genclk_divider |
enum genclk_source |
Generic clock source ID.
Each generic clock may be generated from a different clock source. These are the available alternatives provided by the chip.
|
inlinestatic |
References genclk_config::ctrl.
Referenced by genclk_enable_config(), and main().
|
inlinestatic |
References genclk_config::ctrl.
|
inlinestatic |
References genclk_config::ctrl.
Referenced by genclk_enable_config(), and main().
|
inlinestatic |
Select a new source clock src in configuration cfg.
References genclk_config::ctrl, GENCLK_PCK_SRC_MAINCK_12M_RC, GENCLK_PCK_SRC_MAINCK_4M_RC, GENCLK_PCK_SRC_MAINCK_8M_RC, GENCLK_PCK_SRC_MAINCK_BYPASS, GENCLK_PCK_SRC_MAINCK_XTAL, GENCLK_PCK_SRC_MCK, GENCLK_PCK_SRC_PLLACK, GENCLK_PCK_SRC_PLLBCK, GENCLK_PCK_SRC_SLCK_BYPASS, GENCLK_PCK_SRC_SLCK_RC, and GENCLK_PCK_SRC_SLCK_XTAL.
Referenced by genclk_enable_config(), and main().
|
inlinestatic |
References genclk_config::ctrl.
|
inlinestatic |
References pmc_disable_pck().
|
inlinestatic |
References genclk_config::ctrl, and pmc_enable_pck().
Referenced by genclk_enable_config(), and main().
|
inlinestatic |
Enable the configuration defined by src and divider for the generic clock identified by id.
id | The ID of the generic clock. |
src | The source clock of the generic clock. |
divider | The divider used to generate the generic clock. |
References genclk_config_defaults(), genclk_config_set_divider(), genclk_config_set_source(), genclk_enable(), and genclk_enable_source().
|
inlinestatic |
Enable the source clock src used by a generic clock.
References Assert, GENCLK_PCK_SRC_MAINCK_12M_RC, GENCLK_PCK_SRC_MAINCK_4M_RC, GENCLK_PCK_SRC_MAINCK_8M_RC, GENCLK_PCK_SRC_MAINCK_BYPASS, GENCLK_PCK_SRC_MAINCK_XTAL, GENCLK_PCK_SRC_MCK, GENCLK_PCK_SRC_PLLACK, GENCLK_PCK_SRC_PLLBCK, GENCLK_PCK_SRC_SLCK_BYPASS, GENCLK_PCK_SRC_SLCK_RC, GENCLK_PCK_SRC_SLCK_XTAL, osc_enable(), osc_is_ready(), OSC_MAINCK_12M_RC, OSC_MAINCK_4M_RC, OSC_MAINCK_8M_RC, OSC_MAINCK_BYPASS, OSC_MAINCK_XTAL, OSC_SLCK_32K_BYPASS, OSC_SLCK_32K_RC, OSC_SLCK_32K_XTAL, osc_wait_ready(), and pll_enable_config_defaults().
Referenced by genclk_enable_config().