Clock system example 2 configuration for the A3BU-XPLAINED.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
Example configuration | |
#define | CLKOUT_PORT PORTCFG_CLKOUT_PC7_gc |
Port to output clock signal on. More... | |
#define | IOPORT_PIN IOPORT_CREATE_PIN(PORTC, 7) |
Pin to set as output for clock signal. More... | |
#define CLKOUT_PORT PORTCFG_CLKOUT_PC7_gc |
Port to output clock signal on.
This is the configuration for the clock output port, and must be defined as one of the PORTCFG_CLKOUT_t
settings of the device header file.
Referenced by main().
#define IOPORT_PIN IOPORT_CREATE_PIN(PORTC, 7) |
Pin to set as output for clock signal.
This must be defined as IOPORT pin 7 of the port setting in CLKOUT_PORT.
Referenced by main().