Clock system example 3 configuration for AT32EVK1100.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | LED_EXAMPLE_OUTPUT LED0_GPIO |
Example configuration | |
#define | NEXT_BUTTON GPIO_PUSH_BUTTON_0 |
Pin to use for button input. More... | |
#define | STEP4_PLL_OUTPUT_FREQ 120000000UL |
PLL output frequency for step 4. More... | |
#define LED_EXAMPLE_OUTPUT LED0_GPIO |
Referenced by ISR().
#define NEXT_BUTTON GPIO_PUSH_BUTTON_0 |
Pin to use for button input.
This is the active low pin to use for user input.
Referenced by wait_for_switches().
#define STEP4_PLL_OUTPUT_FREQ 120000000UL |
PLL output frequency for step 4.
This is the frequency to set the PLL to output once the example application reaches step 4 in the clock setting sequence.
Referenced by main().