See Quick Start Guide for the System Clock Management service (UC3B0/UC3B1).
The sysclk API covers the system clock and all clocks derived from it. The system clock is a chip-internal clock on which all synchronous clocks, i.e. CPU and bus/peripheral clocks, are based. The system clock is typically generated from one of a variety of sources, which may include crystal and RC oscillators as well as PLLs. The clocks derived from the system clock are sometimes also known as synchronous clocks, since they always run synchronously with respect to each other, as opposed to generic clocks which may run from different oscillators or PLLs.
Most applications should simply call sysclk_init() to initialize everything related to the system clock and its source (oscillator, PLL or DFLL), and leave it at that. More advanced applications, and platform-specific drivers, may require additional services from the clock system, some of which may be platform-specific.
The sysclk API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.
The following functions are available on all platforms with the same parameters and functionality. These functions may be called freely by portable applications, drivers and services:
The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behavior. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:
All other functions should be considered platform-specific. Enabling/disabling clocks to specific peripherals as well as determining the speed of these clocks should be done by calling functions provided by the driver for that peripheral.
Modules | |
System Clock internals | |
Macros | |
#define | CONFIG_SYSCLK_CPU_DIV 0 |
Configuration symbol for dividing the CPU clock frequency by \(2^{CONFIG\_SYSCLK\_CPU\_DIV}\). More... | |
#define | CONFIG_SYSCLK_INIT_CPUMASK |
Configuration symbol for the CPU clocks enabled at power-on after the sysclock module has been initialized. More... | |
#define | CONFIG_SYSCLK_INIT_HSBMASK |
Configuration symbol for the HSB clocks enabled at power-on after the sysclock module has been initialized. More... | |
#define | CONFIG_SYSCLK_INIT_PBAMASK |
Configuration symbol for the PBA clocks enabled at power-on after the sysclock module has been initialized. More... | |
#define | CONFIG_SYSCLK_INIT_PBBMASK |
Configuration symbol for the PBB clocks enabled at power-on after the sysclock module has been initialized. More... | |
#define | CONFIG_SYSCLK_PBA_DIV 0 |
Configuration symbol for dividing the PBA clock frequency by \(2^{CONFIG\_SYSCLK\_PBA\_DIV}\). More... | |
#define | CONFIG_SYSCLK_PBB_DIV 0 |
Configuration symbol for dividing the PBB clock frequency by \(2^{CONFIG\_SYSCLK\_PBB\_DIV}\). More... | |
#define | CONFIG_SYSCLK_SOURCE SYSCLK_SRC_RCSYS |
#define | CONFIG_USBCLK_DIV |
Configuration symbol for the USB generic clock divider setting. More... | |
#define | CONFIG_USBCLK_SOURCE |
Configuration symbol for the USB generic clock source. More... | |
#define | USBCLK_STARTUP_TIMEOUT (OSC0_STARTUP_TIMEOUT*(1000000/AVR32_PM_RCOSC_FREQUENCY)) |
Number of us to wait for USB clock to start. More... | |
Functions | |
void | sysclk_disable_usb (void) |
Disable the USB generic clock. More... | |
void | sysclk_enable_usb (void) |
Enable the USB generic clock. More... | |
void | sysclk_priv_disable_module (unsigned int bus_id, unsigned int module_index) |
Disable a maskable module clock. More... | |
void | sysclk_priv_enable_module (unsigned int bus_id, unsigned int module_index) |
Enable a maskable module clock. More... | |
System Clock Initialization | |
void | sysclk_init (void) |
Initialize the synchronous clock system. More... | |
System Clock Sources | |
#define | SYSCLK_SRC_RCSYS 0 |
Use slow clock as main clock. More... | |
#define | SYSCLK_SRC_OSC0 1 |
Use OSC0 as main clock. More... | |
#define | SYSCLK_SRC_PLL0 2 |
Use PLL0 as main clock. More... | |
USB Clock Sources | |
#define | USBCLK_SRC_OSC0 GENCLK_SRC_OSC0 |
Use OSC0. More... | |
#define | USBCLK_SRC_PLL0 GENCLK_SRC_PLL0 |
Use PLL0. More... | |
#define | USBCLK_SRC_PLL1 GENCLK_SRC_PLL1 |
Use PLL1. More... | |
Clocks derived from the CPU clock | |
#define | SYSCLK_OCD AVR32_OCD_CLK_CPU |
On-Chip Debug system. More... | |
#define | SYSCLK_SYSTIMER AVR32_CORE_CLK_CPU_COUNT |
COUNT/COMPARE system registers. More... | |
Clocks derived from the HSB clock | |
#define | SYSCLK_FLASHC_DATA (AVR32_FLASHC_CLK_HSB % 32) |
Flash data interface. More... | |
#define | SYSCLK_PBA_BRIDGE (AVR32_HMATRIX_CLK_HSB_PBA_BRIDGE % 32) |
HSB<->PBA bridge. More... | |
#define | SYSCLK_PBB_BRIDGE (AVR32_HMATRIX_CLK_HSB_PBB_BRIDGE % 32) |
HSB<->PBB bridge. More... | |
#define | SYSCLK_USBB_DATA (AVR32_USBB_CLK_HSB % 32) |
USBB DMA and FIFO interface. More... | |
#define | SYSCLK_PDCA_HSB (AVR32_PDCA_CLK_HSB % 32) |
PDCA memory interface. More... | |
Clocks derived from the PBA clock | |
#define | SYSCLK_INTC (AVR32_INTC_CLK_PBA % 32) |
Internal interrupt controller. More... | |
#define | SYSCLK_GPIO (AVR32_GPIO_CLK_PBA % 32) |
General-Purpose I/O. More... | |
#define | SYSCLK_PDCA_PB (AVR32_PDCA_CLK_PBA % 32) |
PDCA peripheral bus interface. More... | |
#define | SYSCLK_PM (AVR32_PM_CLK_PBA % 32) |
PM/RTC/EIM configuration. More... | |
#define | SYSCLK_ADC (AVR32_ADC_CLK_PBA % 32) |
A/D Converter. More... | |
#define | SYSCLK_SPI (AVR32_SPI_CLK_PBA % 32) |
SPI Controller 0. More... | |
#define | SYSCLK_TWI (AVR32_TWI_CLK_PBA % 32) |
TWI Controller. More... | |
#define | SYSCLK_USART0 (AVR32_USART0_CLK_PBA % 32) |
USART 0. More... | |
#define | SYSCLK_USART1 (AVR32_USART1_CLK_PBA % 32) |
USART 1. More... | |
#define | SYSCLK_USART2 (AVR32_USART2_CLK_PBA % 32) |
USART 2. More... | |
#define | SYSCLK_PWM (AVR32_PWM_CLK_PBA % 32) |
PWM. More... | |
#define | SYSCLK_SSC (AVR32_SSC_CLK_PBA % 32) |
Synchronous Serial Controller. More... | |
#define | SYSCLK_TC (AVR32_TC_CLK_PBA % 32) |
Timer/Counter. More... | |
#define | SYSCLK_DAC (AVR32_ABDAC_CLK_PBA % 32) |
D/A Converter. More... | |
Clocks derived from the PBB clock | |
#define | SYSCLK_HMATRIX (AVR32_HMATRIX_CLK_PBB % 32) |
HSB Matrix configuration. More... | |
#define | SYSCLK_USBB_REGS (AVR32_USBB_CLK_PBB % 32) |
USBB registers. More... | |
#define | SYSCLK_FLASHC_REGS (AVR32_FLASHC_CLK_PBB % 32) |
Flash Controller registers. More... | |
Querying the system clock and its derived clocks | |
The following functions may be used to query the current frequency of the system clock and the CPU and bus clocks derived from it. sysclk_get_main_hz() and sysclk_get_cpu_hz() can be assumed to be available on all platforms, although some platforms may define additional accessors for various chip-internal bus clocks. These are usually not intended to be queried directly by generic code. | |
static uint32_t | sysclk_get_main_hz (void) |
Return the current rate in Hz of the main system clock. More... | |
static uint32_t | sysclk_get_cpu_hz (void) |
Return the current rate in Hz of the CPU clock. More... | |
static uint32_t | sysclk_get_hsb_hz (void) |
Return the current rate in Hz of the High-Speed Bus clock. More... | |
static uint32_t | sysclk_get_pba_hz (void) |
Return the current rate in Hz of the Peripheral Bus A clock. More... | |
static uint32_t | sysclk_get_pbb_hz (void) |
Return the current rate in Hz of the Peripheral Bus B clock. More... | |
static uint32_t | sysclk_get_peripheral_bus_hz (const volatile void *module) |
Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral. More... | |
Enabling and disabling synchronous clocks | |
void | sysclk_enable_pbb_module (unsigned int index) |
Enable a module clock derived from the PBB clock. More... | |
void | sysclk_disable_pbb_module (unsigned int index) |
Disable a module clock derived from the PBB clock. More... | |
static void | sysclk_enable_cpu_module (unsigned int index) |
Enable a module clock derived from the CPU clock. More... | |
static void | sysclk_disable_cpu_module (unsigned int index) |
Disable a module clock derived from the CPU clock. More... | |
static void | sysclk_enable_hsb_module (unsigned int index) |
Enable a module clock derived from the HSB clock. More... | |
static void | sysclk_disable_hsb_module (unsigned int index) |
Disable a module clock derived from the HSB clock. More... | |
static void | sysclk_enable_pba_module (unsigned int index) |
Enable a module clock derived from the PBA clock. More... | |
static void | sysclk_disable_pba_module (unsigned int index) |
Disable a module clock derived from the PBA clock. More... | |
static void | sysclk_enable_peripheral_clock (const volatile void *module) |
Enable a peripheral's clock from its base address. More... | |
static void | sysclk_disable_peripheral_clock (const volatile void *module) |
Disable a peripheral's clock from its base address. More... | |
System Clock Source and Prescaler configuration | |
static void | sysclk_set_prescalers (unsigned int cpu_shift, unsigned int pba_shift, unsigned int pbb_shift) |
Set system clock prescaler configuration. More... | |
static void | sysclk_set_source (uint_fast8_t src) |
Change the source of the main system clock. More... | |
#define CONFIG_SYSCLK_CPU_DIV 0 |
Configuration symbol for dividing the CPU clock frequency by \(2^{CONFIG\_SYSCLK\_CPU\_DIV}\).
If this symbol is not defined, the CPU clock frequency is not divided.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_get_cpu_hz(), and sysclk_get_hsb_hz().
#define CONFIG_SYSCLK_INIT_CPUMASK |
Configuration symbol for the CPU clocks enabled at power-on after the sysclock module has been initialized.
By default, all CPU clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx
settings.
If this symbol is not defined, then all CPU clocks are left enabled.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_init().
#define CONFIG_SYSCLK_INIT_HSBMASK |
Configuration symbol for the HSB clocks enabled at power-on after the sysclock module has been initialized.
By default, all HSB clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx
settings.
If this symbol is not defined, then all HSB clocks are left enabled.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_init().
#define CONFIG_SYSCLK_INIT_PBAMASK |
Configuration symbol for the PBA clocks enabled at power-on after the sysclock module has been initialized.
By default, all PBA clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx
settings.
If this symbol is not defined, then all PBA clocks are left enabled.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_init().
#define CONFIG_SYSCLK_INIT_PBBMASK |
Configuration symbol for the PBB clocks enabled at power-on after the sysclock module has been initialized.
By default, all PBB clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx
settings.
If this symbol is not defined, then all PBB clocks are left enabled.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_init().
#define CONFIG_SYSCLK_PBA_DIV 0 |
Configuration symbol for dividing the PBA clock frequency by \(2^{CONFIG\_SYSCLK\_PBA\_DIV}\).
If this symbol is not defined, the PBA clock frequency is not divided.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_get_pba_hz().
#define CONFIG_SYSCLK_PBB_DIV 0 |
Configuration symbol for dividing the PBB clock frequency by \(2^{CONFIG\_SYSCLK\_PBB\_DIV}\).
If this symbol is not defined, the PBB clock frequency is not divided.
This symbol may be defined in conf_clock.h.
Referenced by sysclk_get_pbb_hz().
#define CONFIG_SYSCLK_SOURCE SYSCLK_SRC_RCSYS |
Referenced by sysclk_get_main_hz().
#define CONFIG_USBCLK_DIV |
Configuration symbol for the USB generic clock divider setting.
Sets the clock division for the USB generic clock. If a USB clock source is selected with CONFIG_USBCLK_SOURCE, this configuration symbol must also be defined.
Define this as any value that does not exceed GENCLK_DIV_MAX
, and which will give a 48 MHz clock frequency from the selected source.
#define CONFIG_USBCLK_SOURCE |
Configuration symbol for the USB generic clock source.
Sets the clock source to use for the USB. The source must also be properly configured.
Define this to one of the USBCLK_SRC_xxx
settings. Leave it undefined if USB is not required.
#define SYSCLK_ADC (AVR32_ADC_CLK_PBA % 32) |
A/D Converter.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_DAC (AVR32_ABDAC_CLK_PBA % 32) |
D/A Converter.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_FLASHC_DATA (AVR32_FLASHC_CLK_HSB % 32) |
Flash data interface.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_FLASHC_REGS (AVR32_FLASHC_CLK_PBB % 32) |
Flash Controller registers.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_GPIO (AVR32_GPIO_CLK_PBA % 32) |
General-Purpose I/O.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_HMATRIX (AVR32_HMATRIX_CLK_PBB % 32) |
HSB Matrix configuration.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_INTC (AVR32_INTC_CLK_PBA % 32) |
Internal interrupt controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_OCD AVR32_OCD_CLK_CPU |
On-Chip Debug system.
#define SYSCLK_PBA_BRIDGE (AVR32_HMATRIX_CLK_HSB_PBA_BRIDGE % 32) |
HSB<->PBA bridge.
#define SYSCLK_PBB_BRIDGE (AVR32_HMATRIX_CLK_HSB_PBB_BRIDGE % 32) |
HSB<->PBB bridge.
Referenced by sysclk_disable_pbb_module(), and sysclk_enable_pbb_module().
#define SYSCLK_PDCA_HSB (AVR32_PDCA_CLK_HSB % 32) |
PDCA memory interface.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_PDCA_PB (AVR32_PDCA_CLK_PBA % 32) |
PDCA peripheral bus interface.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_PM (AVR32_PM_CLK_PBA % 32) |
PM/RTC/EIM configuration.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_PWM (AVR32_PWM_CLK_PBA % 32) |
PWM.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_SPI (AVR32_SPI_CLK_PBA % 32) |
SPI Controller 0.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_SRC_OSC0 1 |
Use OSC0 as main clock.
Referenced by main(), sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_SRC_PLL0 2 |
Use PLL0 as main clock.
Referenced by main(), sysclk_get_main_hz(), sysclk_init(), and sysclk_set_source().
#define SYSCLK_SRC_RCSYS 0 |
Use slow clock as main clock.
Referenced by main(), sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_SSC (AVR32_SSC_CLK_PBA % 32) |
Synchronous Serial Controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_SYSTIMER AVR32_CORE_CLK_CPU_COUNT |
COUNT/COMPARE system registers.
#define SYSCLK_TC (AVR32_TC_CLK_PBA % 32) |
Timer/Counter.
Referenced by main(), sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_TWI (AVR32_TWI_CLK_PBA % 32) |
TWI Controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USART0 (AVR32_USART0_CLK_PBA % 32) |
USART 0.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USART1 (AVR32_USART1_CLK_PBA % 32) |
USART 1.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USART2 (AVR32_USART2_CLK_PBA % 32) |
USART 2.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USBB_DATA (AVR32_USBB_CLK_HSB % 32) |
USBB DMA and FIFO interface.
Referenced by sysclk_disable_peripheral_clock(), sysclk_disable_usb(), sysclk_enable_peripheral_clock(), and sysclk_enable_usb().
#define SYSCLK_USBB_REGS (AVR32_USBB_CLK_PBB % 32) |
USBB registers.
Referenced by sysclk_disable_peripheral_clock(), sysclk_disable_usb(), sysclk_enable_peripheral_clock(), and sysclk_enable_usb().
#define USBCLK_SRC_OSC0 GENCLK_SRC_OSC0 |
Use OSC0.
#define USBCLK_SRC_PLL0 GENCLK_SRC_PLL0 |
Use PLL0.
#define USBCLK_SRC_PLL1 GENCLK_SRC_PLL1 |
Use PLL1.
#define USBCLK_STARTUP_TIMEOUT (OSC0_STARTUP_TIMEOUT*(1000000/AVR32_PM_RCOSC_FREQUENCY)) |
Number of us to wait for USB clock to start.
|
inlinestatic |
Disable a module clock derived from the CPU clock.
index | Index of the module clock in the CPUMASK register |
References sysclk_priv_disable_module().
|
inlinestatic |
Disable a module clock derived from the HSB clock.
index | Index of the module clock in the HSBMASK register |
References sysclk_priv_disable_module().
Referenced by sysclk_disable_pbb_module(), sysclk_disable_peripheral_clock(), and sysclk_disable_usb().
|
inlinestatic |
Disable a module clock derived from the PBA clock.
index | Index of the module clock in the PBAMASK register |
References sysclk_priv_disable_module().
Referenced by sysclk_disable_peripheral_clock().
void sysclk_disable_pbb_module | ( | unsigned int | index | ) |
Disable a module clock derived from the PBB clock.
index | Index of the module clock in the PBBMASK register |
References cpu_irq_restore(), cpu_irq_save(), sysclk_disable_hsb_module(), SYSCLK_PBB_BRIDGE, sysclk_pbb_refcount, and sysclk_priv_disable_module().
Referenced by sysclk_disable_peripheral_clock(), and sysclk_disable_usb().
|
inlinestatic |
Disable a peripheral's clock from its base address.
Disables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be disabled also.
module | Pointer to the module's base address. |
References Assert, SYSCLK_ADC, SYSCLK_DAC, sysclk_disable_hsb_module(), sysclk_disable_pba_module(), sysclk_disable_pbb_module(), SYSCLK_FLASHC_DATA, SYSCLK_FLASHC_REGS, SYSCLK_GPIO, SYSCLK_HMATRIX, SYSCLK_INTC, SYSCLK_PDCA_HSB, SYSCLK_PDCA_PB, SYSCLK_PM, SYSCLK_PWM, SYSCLK_SPI, SYSCLK_SSC, SYSCLK_TC, SYSCLK_TWI, SYSCLK_USART0, SYSCLK_USART1, SYSCLK_USART2, SYSCLK_USBB_DATA, and SYSCLK_USBB_REGS.
void sysclk_disable_usb | ( | void | ) |
Disable the USB generic clock.
References genclk_disable(), sysclk_disable_hsb_module(), sysclk_disable_pbb_module(), SYSCLK_USBB_DATA, and SYSCLK_USBB_REGS.
|
inlinestatic |
Enable a module clock derived from the CPU clock.
index | Index of the module clock in the CPUMASK register |
References sysclk_priv_enable_module().
|
inlinestatic |
Enable a module clock derived from the HSB clock.
index | Index of the module clock in the HSBMASK register |
References sysclk_priv_enable_module().
Referenced by sysclk_enable_pbb_module(), sysclk_enable_peripheral_clock(), and sysclk_enable_usb().
|
inlinestatic |
Enable a module clock derived from the PBA clock.
index | Index of the module clock in the PBAMASK register |
References sysclk_priv_enable_module().
Referenced by main(), and sysclk_enable_peripheral_clock().
void sysclk_enable_pbb_module | ( | unsigned int | index | ) |
Enable a module clock derived from the PBB clock.
index | Index of the module clock in the PBBMASK register |
References cpu_irq_restore(), cpu_irq_save(), sysclk_enable_hsb_module(), SYSCLK_PBB_BRIDGE, sysclk_pbb_refcount, and sysclk_priv_enable_module().
Referenced by sysclk_enable_peripheral_clock(), and sysclk_enable_usb().
|
inlinestatic |
Enable a peripheral's clock from its base address.
Enables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be enabled also.
module | Pointer to the module's base address. |
References Assert, SYSCLK_ADC, SYSCLK_DAC, sysclk_enable_hsb_module(), sysclk_enable_pba_module(), sysclk_enable_pbb_module(), SYSCLK_FLASHC_DATA, SYSCLK_FLASHC_REGS, SYSCLK_GPIO, SYSCLK_HMATRIX, SYSCLK_INTC, SYSCLK_PDCA_HSB, SYSCLK_PDCA_PB, SYSCLK_PM, SYSCLK_PWM, SYSCLK_SPI, SYSCLK_SSC, SYSCLK_TC, SYSCLK_TWI, SYSCLK_USART0, SYSCLK_USART1, SYSCLK_USART2, SYSCLK_USBB_DATA, and SYSCLK_USBB_REGS.
void sysclk_enable_usb | ( | void | ) |
Enable the USB generic clock.
References CONFIG_USBCLK_DIV, CONFIG_USBCLK_SOURCE, genclk_enable_config(), sysclk_enable_hsb_module(), sysclk_enable_pbb_module(), SYSCLK_USBB_DATA, and SYSCLK_USBB_REGS.
|
inlinestatic |
Return the current rate in Hz of the CPU clock.
References CONFIG_SYSCLK_CPU_DIV, and sysclk_get_main_hz().
Referenced by sysclk_init().
|
inlinestatic |
Return the current rate in Hz of the High-Speed Bus clock.
References CONFIG_SYSCLK_CPU_DIV, and sysclk_get_main_hz().
|
inlinestatic |
Return the current rate in Hz of the main system clock.
References BOARD_OSC0_HZ, CONFIG_SYSCLK_SOURCE, OSC_SLOW_NOMINAL_HZ, pll_get_default_rate, SYSCLK_SRC_OSC0, SYSCLK_SRC_PLL0, and SYSCLK_SRC_RCSYS.
Referenced by sysclk_get_cpu_hz(), sysclk_get_hsb_hz(), sysclk_get_pba_hz(), and sysclk_get_pbb_hz().
|
inlinestatic |
Return the current rate in Hz of the Peripheral Bus A clock.
References CONFIG_SYSCLK_PBA_DIV, and sysclk_get_main_hz().
Referenced by sysclk_get_peripheral_bus_hz().
|
inlinestatic |
Return the current rate in Hz of the Peripheral Bus B clock.
References CONFIG_SYSCLK_PBB_DIV, and sysclk_get_main_hz().
Referenced by sysclk_get_peripheral_bus_hz().
|
inlinestatic |
Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral.
module | Pointer to the module's base address. |
References Assert, sysclk_get_pba_hz(), and sysclk_get_pbb_hz().
void sysclk_init | ( | void | ) |
Initialize the synchronous clock system.
This function will initialize the system clock and its source. This includes:
Since all non-essential peripheral clocks are initially disabled, it is the responsibility of the peripheral driver to re-enable any clocks that are needed for normal operation.
References Assert, BOARD_OSC0_HZ, CONFIG_SYSCLK_CPU_DIV, CONFIG_SYSCLK_INIT_CPUMASK, CONFIG_SYSCLK_INIT_HSBMASK, CONFIG_SYSCLK_INIT_PBAMASK, CONFIG_SYSCLK_INIT_PBBMASK, CONFIG_SYSCLK_PBA_DIV, CONFIG_SYSCLK_PBB_DIV, CONFIG_SYSCLK_SOURCE, flash_set_bus_freq, osc_enable(), OSC_ID_OSC0, osc_wait_ready(), pll_enable_config_defaults(), sysclk_get_cpu_hz(), SYSCLK_INIT_MINIMAL_CPUMASK, SYSCLK_INIT_MINIMAL_HSBMASK, SYSCLK_INIT_MINIMAL_PBAMASK, SYSCLK_INIT_MINIMAL_PBBMASK, sysclk_set_prescalers(), sysclk_set_source(), SYSCLK_SRC_OSC0, SYSCLK_SRC_PLL0, and SYSCLK_SRC_RCSYS.
Referenced by main().
void sysclk_priv_disable_module | ( | unsigned int | bus_id, |
unsigned int | module_index | ||
) |
Disable a maskable module clock.
bus_id | Bus index, given by the AVR32_PM_CLK_GRP_xxx definitions. |
module_index | Index of the module to be disabled. This is the bit number in the corresponding xxxMASK register. |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by sysclk_disable_cpu_module(), sysclk_disable_hsb_module(), sysclk_disable_pba_module(), and sysclk_disable_pbb_module().
void sysclk_priv_enable_module | ( | unsigned int | bus_id, |
unsigned int | module_index | ||
) |
Enable a maskable module clock.
bus_id | Bus index, given by the AVR32_PM_CLK_GRP_xxx definitions. |
module_index | Index of the module to be enabled. This is the bit number in the corresponding xxxMASK register. |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by sysclk_enable_cpu_module(), sysclk_enable_hsb_module(), sysclk_enable_pba_module(), and sysclk_enable_pbb_module().
|
inlinestatic |
Set system clock prescaler configuration.
This function will change the system clock prescaler configuration to match the parameters.
cpu_shift | The CPU clock will be divided by \(2^{cpu\_shift}\) |
pba_shift | The PBA clock will be divided by \(2^{pba\_shift}\) |
pbb_shift | The PBB clock will be divided by \(2^{pbb\_shift}\) |
References Assert.
Referenced by main(), and sysclk_init().
|
inlinestatic |
Change the source of the main system clock.
src | The new system clock source. Must be one of the constants from the System Clock Sources section. |
References Assert, cpu_irq_restore(), cpu_irq_save(), and SYSCLK_SRC_PLL0.
Referenced by main(), and sysclk_init().