Clock system example 3 configuration for SAM4L8 Xplained Pro.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | LED_EXAMPLE_OUTPUT LED_0_PIN |
This is the LED that will be toggled in this example. More... | |
Example configuration | |
#define | NEXT_BUTTON BUTTON_0_PIN |
Pin to use for button input. More... | |
#define LED_EXAMPLE_OUTPUT LED_0_PIN |
This is the LED that will be toggled in this example.
Referenced by SysTick_Handler().
#define NEXT_BUTTON BUTTON_0_PIN |
Pin to use for button input.
This is the pin for the onboard PB0 button, corresponding to PC03.
This is the active low pin to use for user input.
Referenced by wait_for_switches().