Microchip® Advanced Software Framework

conf_spi_master_example.h File Reference
#include "conf_board.h"
#include "sysclk.h"

Macros

Configuration
#define SPI_EXAMPLE   AT45DBX_SPI
 
#define SPI_DEVICE_EXAMPLE_ID   AT45DBX_SPI_NPCS
 
#define SPI_EXAMPLE_BAUDRATE   12000000
 
#define SPI_EXAMPLE_LED_PIN_EXAMPLE_1   LED0_GPIO
 
#define SPI_EXAMPLE_LED_PIN_EXAMPLE_2   LED1_GPIO
 

#define SPI_DEVICE_EXAMPLE_ID   AT45DBX_SPI_NPCS
#define SPI_EXAMPLE   AT45DBX_SPI

Referenced by main(), and spi_at45dbx_mem_check().

#define SPI_EXAMPLE_BAUDRATE   12000000

Referenced by main().

#define SPI_EXAMPLE_LED_PIN_EXAMPLE_1   LED0_GPIO

Referenced by main().

#define SPI_EXAMPLE_LED_PIN_EXAMPLE_2   LED1_GPIO

Referenced by main().