- intro Introduction
- This example demonstrates how to use the SPI Master Mode Basic Services.
- files Main Files
-
- spiapiinfo services/basic/spi API
- The spi API can be found here.
- deviceinfo Device Info
- This example has been tested with the following setup:
- Evaluation kits with a serialflash (AT25 series) connected through an SPI interface.
- exampledescription Description of the example
-
- compinfo Compilation Info
- This software was written for the GNU GCC and IAR for AVR and SAM. Other compilers may or may not work.
- contactinfo Contact Information
- For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/